Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi with WS2812b strips
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 707 subscribers
  • Views 4453 views
  • Users 0 members are here
Related

Raspberry Pi with WS2812b strips

e14 Contributor
e14 Contributor over 12 years ago

Hi

       I am looking for advice regarding feasibility and future errors that I may face for my project. I am trying to control 300 led strips from Adafruit available at http://www.adafruit.com/products/1138

 

These strip require an input at voltage level 5V. I know that I must use a 3.3V to 5V voltage converter  to keep both strips and Pi safe.

 

IS there anything that I should be careful about?

 

Please help.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello guys, once again thank you for your valuable replies.

     

    First of all :- Yes I am trying to make a display out of this project. So definitely I am using 18000 leds.  Cost is not my problem. I can get a strip from www.alibaba.com for $9/- with 60 leds per meter.

     

    Here is my "theoretical" calculations:-

     

    (Basic assumption is Pi can used to create a delay of 50 n seconds when it is over clocked at 1.2GHz)

     

    To send one bit data to strip (either 0 or 1) time required = 1.25 u seconds

    to send one byte, time required = 1.25 x 8 = 10 u seconds

    to semd 24 bytes i.e. one pixel value, time required = 10 x 3 = 30 u seconds

     

     

     

    • Assume refresh rate = 50 Hz

    time for one frame = 1000/50 = 20 m seconds

    reset pulse time = 80 u seconds (Assume) (>50 u seconds required)

    consider x is max no. of pixels, then

     

    (x*30)+80   = 20000

    x*30          = 19920

    x = 664

     

    So max no of leds per pin on Pi is 664.

    8 pins are available on Pi. So max no of leds per Pi = 664*8 = 5312


    • Assume refresh rate = 25 Hz

    time for one frame = 1000/25 = 40 m seconds

    reset pulse time = 70 u seconds (Assume) (>50 u seconds required)

    consider x is max no. of pixels, then

     

    (x*30)+70   = 40000

    x*30          = 39930

    x = 1331

     

    So max no of leds per pin on Pi is 1331.

    8 pins are available on Pi. So max no of leds per Pi = 1331*8 = 10648.

     

     

    This is my theory. Please tell me if it would work!


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello guys, once again thank you for your valuable replies.

     

    First of all :- Yes I am trying to make a display out of this project. So definitely I am using 18000 leds.  Cost is not my problem. I can get a strip from www.alibaba.com for $9/- with 60 leds per meter.

     

    Here is my "theoretical" calculations:-

     

    (Basic assumption is Pi can used to create a delay of 50 n seconds when it is over clocked at 1.2GHz)

     

    To send one bit data to strip (either 0 or 1) time required = 1.25 u seconds

    to send one byte, time required = 1.25 x 8 = 10 u seconds

    to semd 24 bytes i.e. one pixel value, time required = 10 x 3 = 30 u seconds

     

     

     

    • Assume refresh rate = 50 Hz

    time for one frame = 1000/50 = 20 m seconds

    reset pulse time = 80 u seconds (Assume) (>50 u seconds required)

    consider x is max no. of pixels, then

     

    (x*30)+80   = 20000

    x*30          = 19920

    x = 664

     

    So max no of leds per pin on Pi is 664.

    8 pins are available on Pi. So max no of leds per Pi = 664*8 = 5312


    • Assume refresh rate = 25 Hz

    time for one frame = 1000/25 = 40 m seconds

    reset pulse time = 70 u seconds (Assume) (>50 u seconds required)

    consider x is max no. of pixels, then

     

    (x*30)+70   = 40000

    x*30          = 39930

    x = 1331

     

    So max no of leds per pin on Pi is 1331.

    8 pins are available on Pi. So max no of leds per Pi = 1331*8 = 10648.

     

     

    This is my theory. Please tell me if it would work!