Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum My review of the Wolfson audio card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 1166 views
  • Users 0 members are here
  • wolfson
  • raspberry_pi
  • raspberrypi
  • raspeberry_pi_accessories
  • audio-card
Related

My review of the Wolfson audio card

e14 Contributor
e14 Contributor over 12 years ago

Hello!

 

I received my audio card at the beginning of the week, and I wanted to share my first impressions with you.

 

My needs are pretty simple : I want to use a RaspberryPi and LogitechMediaServer/Squeezelite to listen to music on my HIFI installation. I searched the web for some USB DACs, custom board for Rpi,... but they were too expensive, or they were shipped from US or China (I live in Belgium),... So, I was happy to find one that was not too expensive, and easily shipped to my home.

 

It's shipped in a little cardboard box, the packaging is similar to the one of the RasberryPi itself.

 

The connection with the RaspberryPi is very easy, as you don't need to solder the connector P5. The only issue (not really...), is that the sound card is a little bent because it touches the audio jack of the RaspberryPi.... Any way, if you use the little screw (provided in the box) to maintain the card in place, their should not be any problem.

 

I didn't try to compile the drivers and software by myself, but I hope that they will be integrated in the mainstream Raspbian distribution ASAP. Instead, I downloaded the full OS image available on the website. I had to be patient... it's a 4Go ZIP file which seems to create a 6Go filesystem. Fortunately, I had a 8Go SD card laying around!

 

The OS image boots directly to the graphical interface. I tried to play the HD tracks as explained in the user manual, but then, the rPi would become verry slow, and the CPU was 100% used... Anyway, I tried to read some MP3 file with command like (mpg123), and it works great. I tried the analog and digital output. The sound quality is quite good, far better than the audio output of the raspberryPi!

 

And then I installed Logitech Media Server and Squeezelite. Since then, it is connected to my hifi amplifier and works great!

 

So, appart from the little mechanical problem (the board that touches the audio connector of the rpi), the software the is not (yet) integrated in Raspbian, and the absence of a specific enclosure, I would say that it is a very good product!

 

I didn't try any audio input and recording, though...

 

I wrote an article on my blog in French and English, if you wish to read it ;-)

 

And you, what do you think of this board?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Jean-François Milants, thank you for this review! Squeezebox with LMS and Squeezelite is part of my intended usage scenario, since the Touch is no longer available. You say the RPi became very slow with the HD files, using the processor 100%, but did they play alright? Or did it drop out, fail bits etc? When you played back over LMS, was that 16/44.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I had the issue with the HD files when I tried to play the HD files that are available on the OS image as demo files. I tried to read them using the graphical media player that was on the desktop (I forgot its name), but then, the rpi became very slow and the playback was laggy, there were drops,...

     

    But most of my music is in MP3, or comes from web streams, so, this is not a big deal for me, and I didn't try to understand why the playback of the HD files failed.

     

    Also, I didn't try to read these HD files with LMS...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    The card works really fine, though it needs a lot of tweaking in my case. I use it for a little open source/open hardware project (http://blog.georgmill.de).  The raspberry pi has a realtime enabled kernel running on it. It is connected to an arduino via usb. The arduino produces midi signals which can be used with linux midi software to produce excellent sound together with the wolfson audio card. I tried to capture sound from the built in mics and ... it works. The sound isn't really convincing uses these little onboard mics, but it works. The HD Audio files run without stuttering in vlc http://www.videolan.org/vlc/ In my case they are stored directly on the 8GB MicroSD-Card. I tried to run some WAV and MP3 files from my NAS (WD MyBookLive) . Everything works fine. I am really surprised of what this little audio card can do for you. Read all the PDF docs

    http://www.element14.com/community/docs/DOC-65685/l/data-sheet-of-wm5102

    http://www.element14.com/community/docs/DOC-65674/l/wolfson-datasheet-for-for-wm5102-audio-hub-codec-with-voice-processor-dsp

    http://www.element14.com/community/docs/DOC-65675/l/wolfson-product-brief-for-wm5102-audio-hub-codec-with-voice-processor-dsp

    http://www.element14.com/community/docs/DOC-65691/l/user-manual-for-wolfson-audio-card

    and be surprised ;-)