It appears that the Wolfson drivers will not be in the next Raspbian update.
- (from Raspberry Pi • View topic - Next firmware tree is now 3.12)
- I hope someone from Wolfson reads this and follows up.
It appears that the Wolfson drivers will not be in the next Raspbian update.
Commits are here:
HifiBerry and IQ Audio I2S devices are supported. No Wolfson support until they submit a PR.
Hi Paul Garcia
I have same problem
So
I need your help
Would you tell me how to setup XBMC Gotham?
Can I install raspbmc-2013-12-23.img first,and update the XBMC?
I search the XBMC
in this post
http://forum.xbmc.org/showthread.php?tid=176043&page=80
wget -O xbmc-14-20140420-nc3.tar.gz http://goo.gl/tNRTO0 --no-check-certificate
pv xbmc-14-20140420-nc3.tar.gz | tar xzf - -C /home/pi/.upgrade
sudo cp /home/pi/.upgrade/xbmc-14-20140420-nc3/{fixup_x.dat,start_x.elf} /boot
ln -sfn /home/pi/.upgrade/xbmc-14-20140420-nc3/xbmc-bcm /home/pi/.xbmc-current
sudo reboot
so
my step will working?
I did see this post on Raspbmc from 4/14/2014 so it is coming I would follow this post and possibly recommend Raspbmc as it the only build I am aware of that is building in support. Please let me know if the other builds also offer support or intend to Raspbmc » New Raspbmc update!
I’m adding support for the following sound cards:
- Wolfson Microelectronics Raspberry Pi Module – Wolfson’s patches for this had issues, so I’ve done my best to manually resolve these myself. I have reached out to a developer at Wolfson who tells me patches will be released in the future.
Here is the best solution I can find
The Wolfson audio card doesn't work with the official raspberry pi kernel, and their patches don't apply to the current kernel tree (you have to apply them to a tree from before Christmas).I think your only possibility is to use the supplied sdcard image they distribute, and then follow this:http://www.raspberrypi.org/forums/viewto...61#p520212to get raspmbc working. Note, this is a hack and you will find things that don't work (e.g. updates), but I don't think there is a better solution for now.
Post found How do I get a wolfson audio card working in Raspbmc?
Element14 or Woolfson Do you have a comment on this. At the moment I cannot use the card I bought as I need to run it with the current Kernel.
I think in order to be of any assistance what requirements do you exactly need. What benefits over the older Kernel would you receive vs building it off the newer Kernel. (Note newer Kernel does not always equate to making your project better. Need to see what improvements were made.) Yes there does need to be integration into the default Raspbian images, etc.. But there are almost always options available through a Google search where work outside an official release results in what you need.
By defining why you need to run it with the current Kernel they can answer if any updates that do come out will address your particular need.
The Woolfson card is just part of my system. I need to keep other bits up to date. Having a system where I cannot run apt-get update and / or raspi-update is unacceptable.
You have identified one problem raspi-update? I am not familiar with this I am going to guess you meant rpi-update. rpi-update will update you to the development Kernel. This is not intended for general use. But for the Linux dev's to test out the newer builds to see what bugs need to be discovered before being released into the general public. It's an advanced update utility and I strongly discourage anyone from using it if they want the most reliable tested kernel running on the Pi.
Here is a quote from recantha's blog: http://www.recantha.co.uk/blog/?p=7316
"As others have commented, rpi-update is useful if you want the latest, latest, latest version of the firmware, but does carry with it a few risks to the stability of your system."
This is why you will see files inside this firmware being updated almost daily. Yet the official image is released only a few times each year.
https://github.com/raspberrypi/firmware
https://github.com/Hexxeh/rpi-update
Updating for the sake of updating is never recommended unless your willing to post what issues you encountered and downgrade or help resolve the issues with the new firmware.
No developer should be blamed if raspi-update causes a conflict as they may have just barely downloaded it and began to work on a resolution. kernel: Bump to 3.12.19 is Three days old just how fast a resolution to a developers hardware or software is acceptable?
apt-get update doesn't do anything that should break your system:
apt-get update doesn't actually install new versions of software.
apt-get update downloads the package lists from the repositories and "updates" them to get information on the newest versions of packages and their dependencies. It will do this for all repositories and PPAs.
apt-get upgrade will fetch new versions of packages existing on the machine if APT knows about these new versions by way of apt-get update.
If using apt-get upgrade. Always pay attention to what packages have been updated and report a package that has possibly broken a known working feature. Again downgrade that app and await an official update.
What is holding up the PR Documentation the Foundation needs is unclear and yes Wolfson should act as quickly as possible to get their card into the official Current Release of Raspbian. But as we are unaware of what steps they need to resolve at best we can hope for an update to their progress.
The original question of this thread comes from this post Raspberry Pi • View topic - Next firmware tree is now 3.12
If you notice it was stated the firmware would come out sometime this month I am not sure if it has already or if it is still in progress. Once Wolfson finishes their PR the Foundation will gladly update and include it very quickly.
If you are using this Kernel Dom wrote "Note: this tree is aimed at testers. There could be missing kernel modules, or things that don't work. If you find any problems, then report here, or create a github issue."
Wolfson was commented on and he replied what is needed. This was less than 30 days ago.
Todd Cowley wrote:
What is holding up the PR Documentation the Foundation needs is unclear and yes Wolfson should act as quickly as possible to get their card into the official Current Release of Raspbian. But as we are unaware of what steps they need to resolve at best we can hope for an update to their progress.
Wolfson has been taken over by Cirrus Logic. See this link http://www.bbc.co.uk/news/uk-scotland-scotland-business-27202322
The article says;
"Wolfson has reported losses recently due to volatility in supplying that market.
It has been shedding staff to bring its costs down"
That may have something to do with lack of progress on getting the drivers included in the official Raspbian distribution. If the card is not considered a priority by Cirrus then we may be waiting a long time for anything to happen.
I think there is still hope just posted this:
I came across the following tweet I am hoping for some exciting news and updates.
Looking for an introduction to the Wolfson Audio Card? Join our webinar with @element14 on 12 June to find out more http://bit.ly/1ucIXtF
Wolfson invites you to delve into a new dimension of Raspberry Pi audio with the Wolfson audio card accessory. The Webinar will provide you a detailed overview of the Wolfson Audio Card and also show you creative ways of enhancing your Pi Projects with the use of this leading edge Pi accessory.
Todd Cowley wrote:
I think there is still hope just posted this:
That's encouraging. I guess there will be a period where Cirrus will be reviewing the projects that Wolfson have been engaged in, and decide what they want to do with them going forward. From what I read the Wolfson chief guy is staying on for now to guide the transition.
Todd Cowley wrote:
I'll keep looking for links. What is your desired setup with XBMC? Just curious as a $5 USB Sound card card can deliver the same audio quality out. Here's a good understanding of what this card is compared to a USB sound card. https://www.youtube.com/watch?v=VU-JMVkbCP8&feature=youtu.be I am working on a write up as we speak and testing it out.
My desired setup is XBMC -> Wolfson DAC -> vintage Harman-Kardon receiver. I've tried a $5 USB sound card and it didn't fulfill my needs for several reasons. First, since it runs off the relatively dirty +5V from the Pi, this raises the noise floor to an objectionable level, unless you provide your own dedicated power supply for the USB DAC to run on. Second, since it goes over USB, anything else that goes over USB and generates traffic on that bus (e.g. WiFi adapter, external hard drive) opens the possibility for contention, lag, and skips/pops. (Hence distributions like Volumio that use the RT patch and are highly tuned to avoid this issue.) The Wolfson card, as well as the HiFiBerry, communicate with the Pi using I2S, a dedicated channel that does not suffer from this issue.
Todd Cowley wrote:
I'll keep looking for links. What is your desired setup with XBMC? Just curious as a $5 USB Sound card card can deliver the same audio quality out. Here's a good understanding of what this card is compared to a USB sound card. https://www.youtube.com/watch?v=VU-JMVkbCP8&feature=youtu.be I am working on a write up as we speak and testing it out.
My desired setup is XBMC -> Wolfson DAC -> vintage Harman-Kardon receiver. I've tried a $5 USB sound card and it didn't fulfill my needs for several reasons. First, since it runs off the relatively dirty +5V from the Pi, this raises the noise floor to an objectionable level, unless you provide your own dedicated power supply for the USB DAC to run on. Second, since it goes over USB, anything else that goes over USB and generates traffic on that bus (e.g. WiFi adapter, external hard drive) opens the possibility for contention, lag, and skips/pops. (Hence distributions like Volumio that use the RT patch and are highly tuned to avoid this issue.) The Wolfson card, as well as the HiFiBerry, communicate with the Pi using I2S, a dedicated channel that does not suffer from this issue.
My desired setup is XBMC -> Wolfson DAC -> vintage Harman-Kardon receiver.
You could try my experimental OpenELEC build:
http://www.horus.com/~hias/tmp/openelec-wolfson/
This is OpenELEC 4.0 with kernel 3.10.25 and the Wolfson driver plus the "use case" scripts and a few minor modifications so that the Wolfson card should work out of the box. I just uploaded a new build (20140514) based on the OpenELEC 4.0.1 release.
Please note:
This is an experimental build, although it works for me it could well have bugs.
Especially USB devices might be problematic due to the old kernel.
I don't think the Wolfson driver supports AC3 passthrough, maybe it does, but I can't test it - I'm using only an external stereo DAC.
so long,
Hias
Awesome, thank you so much! I'll give it a try this evening and let you know how it works.
Best,
Ben
This seems very promising and projects upstream by end of June at the latest as that's the last day of Q2. Which should then allow all the Media Center Teams time to implement on their schedule which typically I don't think they sleep much. Hope this alleviates some of the stress and frustration anyone may be feeling. I hope to always give the benefit of the doubt with reputable companies that they hold true and won't release a statement like this unless they were 100% confident in it.
Hi Todd,
Thank you very much for contacting us with regards to the Wolfson audio card for the Raspberry Pi. We are glad to hear that you are a fan of the card and look forward to integrating within projects in the future.
With regards to the PR activity for the Raspberry Pi foundation our plans were to release the board with working software which we have now completed and in parallel work on up streaming the device drivers to the Raspberry Pi foundation. We are executing to this plan and will make our software available for up streaming in Q2 2014. I can confirm we are track to achieve this at present.
I hope you find the audio capability of the audio card exceeds your expectations, we have certainly found that it adds a completely new dimension to the audio possibilities of the Raspberry Pi.
We would of course appreciate any feedback you would like to provide in advance of publishing your review for us to consider.
Best regards,
Wolfson team
Lynn Mason
Sales Administration Manager
Wolfson Microelectronics, Inc.
Santa Clara, CA 95050
Guys feel free to let me know. Direct Message here I prefer to support@raspians.com if you like please put Wolfson Audio Card (Whatever else) in the subject line and I'll start compiling and researching what is known vs what is yet to be revealed.
Put whatever as to what questions you may have as I can't test every single scenario or device. I'll put AC3 passthrough on the list. If you field other questions anywhere else or see other questions I would love the input.
Todd Cowley wrote:
This seems very promising and projects upstream by end of June at the latest as that's the last day of Q2. Which should then allow all the Media Center Teams time to implement on their schedule which typically I don't think they sleep much. Hope this alleviates some of the stress and frustration anyone may be feeling. I hope to always give the benefit of the doubt with reputable companies that they hold true and won't release a statement like this unless they were 100% confident in it.
I hope you are right. However we have been here before http://www.element14.com/community/message/107217/l/re-wolfson-modified-noobs-raspbian-zipped-img-cannot-unzip-new-download#107217
In that post Andy Laing (I think from Element14) said;
"We are currently working with the developers at Wolfson and the RPI Foundation to get the drivers uploaded into the official Raspbian Kernel.
This download image is only ever intended to be a temporary measure, and we will be removing this image as soon as the Wolfson drivers are embedded into the official Raspbian kernel. Once complete, you will only need to do an "apt-get upgrade" to download the kernel drivers for this audio card.
We are expecting this work to be completed within the coming weeks and I will update this thread again once this is completed and provide instructions on how to update your standard Raspbian builds to install the new drivers and additional software needed to run the Wolfson audio card."
That was posted by Andy Laing on March 24th. Note he said that they were expecting the work to be completed 'within the coming weeks'. You would have thought therefore that 6 or 7 weeks later we should not still be waiting for something to happen, and with no further word from Wolfson or Element14 (until you prodded them).
I'd take 'within the coming weeks' to mean 2 or 3 weeks, not 6 or 7. Or indeed probably more weeks yet to come. That sounds like 'months' to me.
Works great, and to top it all off, my USB WiFi dongle works out of the box (I had to compile a kernel module for it before). Thanks!
I agree, this is ridiculous. I bought the card with the understanding that the drivers would be in the kernel within weeks. I am now still waiting.
Wolfson needs to get their act together
Worth the wait, WAC sound better than the hifiberry plus the internal class D amplifier drive loud speakers with no issue , gone thru all the testing, ready to set up my whole house audio.
Juan Gevara wrote:
Worth the wait, WAC sound better than the hifiberry plus the internal class D amplifier drive loud speakers with no issue , gone thru all the testing, ready to set up my whole house audio.
I don't think anybody here thinks the Wolfson isn't a good product, it's just that the good work that has been done on it is being let down by poor support.
There's a few problems
Well, the 4.4Gb download was supposed to be only a temporary solution, not a permanent one. Towards the end of March we were told that work was being done to get the Wolfson drivers included in the standard Raspian distribution 'in the next weeks'. However, we are still waiting for that. The drivers weren't included in the recent Raspian update. If the drivers are included in Raspian then presumably you can do a normal update. If the foundation moves to Jessie then a further update will be required (for the Wolfson driver).
It's not a satisfactory situation,and this is what we are complaining about. I don't know if we've ever had a comment from Wolfson in this forum, and certainly precious few from Element14.
Have you noticed that Ragnar Jensen has already produced a stripped-down version of the Wolfson download? A number of us are using that.