Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 新手如何开始树莓派
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 674 subscribers
  • Views 1253 views
  • Users 0 members are here
Related

新手如何开始树莓派

Former Member
Former Member over 11 years ago

树莓派买回来时候什么都用不了,需要自己买个SD卡,还有自己喜欢的配件,都可以从易络盟这里采购.

 

一.准备工作:

1.最好最准备一张4G以上的SD卡,最好是高速卡,推荐Class4以上的卡,因为卡得速度直接影响树莓派的运行速度.

2.下载树莓派debian系统镜像文件,地址如下:

 

英文下载地址:http://www.raspberrypi.org/downloads

中文下载地址:http://www.52pi.net/forum.php?mod=viewthread&tid=755

 

3.WinXP和Win7下安装镜像的工具win32diskimager,或者USB Image Tool,这个在各大网站都有下载.


4.用win32diskimager在windows下将镜像文件写入SD卡中,打win32diskimager找到镜像文件,选好SD卡盘符,点写入,成功后,点退出.

 

image

 

二.启动系统用SD卡

将SD卡插入树莓派插槽中,连接电源,USB键盘,HDMI到电脑显示器或电视接口,在显示器或电视中后有图形显示,Pi就安装完成,是不是很简单.

 

当然,有了Pi要干嘛?当然玩啊,各种玩法.比如可以烧录XBMC OpenELEC系统,100M左右,开机神速,各种快.

 

系统名字 : OpenElec 中文社区版

系统大小 : 78.52M

简要介绍 : 官方的有个缺点,就是要有Linux才能安装,这个直接烧写,和烧写Raspbian一样简单,用户名是root,密码是openelec,界面还是英文的,汉化优化版稍后奉上.

推荐程度 : HeartsHeartsHeartsHearts

下载地址: 这儿猛击,中文哦,也有英文的.

 

当然还有很多玩法,在树莓派官方,易络盟论坛,以及各种树莓派中文社区都有很多介绍的.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    Google translate will not handle this

     

    can you please post in English

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Robert Peter Oakes

    When you buy a Raspberry Pi,you need to buy a SD card and other accessories which you like~

    First,ready to work:

    1,Ready an SD card which the storge larger than 4GB.If you have a high speed card,that's better.You should use the level Class4 SD card or better,because the card's I/O speed determine the running speed of the Raspberry Pi!

    2,Download the system image(Debain) for the Raspberry Pi,this is tha adress

    English version:Downloads | Raspberry Pi

    Chinese versino:树莓派常用镜像下载 - 发行版讨论组 - 树莓派创客社区 - 手机版 - Powered by Discuz!

    3,Install the win32diskimager on WinXP or Win7.This tool can hep you to install the system of Raspberry Pi.

    4,Open the  win32diskimager and select the image(remember to choose the right disk),them,click "Write"and wait for a minutes,it will note you succeed.

     

    Second,boot from the SD card

    Push the SD card to the slot and connect the power,USBkeyboard,HDMI cable.If the display print the graphic,your Raspberry Pi is working! It's really easy,right?

    So,you have a Pi and what do you want to do?Of course,you can use it to do many thing! For example you can install the XBMC and OpenELCL.Those system can staring up in a shot time

     

    System image:OpenElec(Chinese Version)

    Size:78.52M

    Infomation:if you want to use the offical versino OpenELEC,you must install it on Linux!But the Chinese versino,you can use win32diskimager to install,just like install the Raspbain~

    Feel good:HeartsHeartsHeartsHearts

    Download:这儿猛击,中文哦,也有英文的.(also the official version)

    Robert Peter Oakes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to Robert Peter Oakes

    When you buy a Raspberry Pi,you need to buy a SD card and other accessories which you like~

    First,ready to work:

    1,Ready an SD card which the storge larger than 4GB.If you have a high speed card,that's better.You should use the level Class4 SD card or better,because the card's I/O speed determine the running speed of the Raspberry Pi!

    2,Download the system image(Debain) for the Raspberry Pi,this is tha adress

    English version:Downloads | Raspberry Pi

    Chinese versino:树莓派常用镜像下载 - 发行版讨论组 - 树莓派创客社区 - 手机版 - Powered by Discuz!

    3,Install the win32diskimager on WinXP or Win7.This tool can hep you to install the system of Raspberry Pi.

    4,Open the  win32diskimager and select the image(remember to choose the right disk),them,click "Write"and wait for a minutes,it will note you succeed.

     

    Second,boot from the SD card

    Push the SD card to the slot and connect the power,USBkeyboard,HDMI cable.If the display print the graphic,your Raspberry Pi is working! It's really easy,right?

    So,you have a Pi and what do you want to do?Of course,you can use it to do many thing! For example you can install the XBMC and OpenELCL.Those system can staring up in a shot time

     

    System image:OpenElec(Chinese Version)

    Size:78.52M

    Infomation:if you want to use the offical versino OpenELEC,you must install it on Linux!But the Chinese versino,you can use win32diskimager to install,just like install the Raspbain~

    Feel good:HeartsHeartsHeartsHearts

    Download:这儿猛击,中文哦,也有英文的.(also the official version)

    Robert Peter Oakes