Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Arrêt / Redémarrage Raspberry
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 709 subscribers
  • Views 1246 views
  • Users 0 members are here
Related

Arrêt / Redémarrage Raspberry

e14 Contributor
e14 Contributor over 12 years ago

Bonjour,

 

Je souhaiterais savoir s'il existe une solution pour arrêter proprement le Raspberry et le redémarrer.

 

Nous avons jusqu'ici débranché électriquement le Raspberry, les cartes SD sont désormais corrompues, ce qui n'est pas étonnant.

 

J'aimerai donc savoir s'il existait une solution pour arrêter proprement et/ou redémarrer le raspberry, peut-être un bouton poussoir ou quelque chose de ce type pour éviter d'endommager les cartes SD.

 

Evidemment je connais les commandes suivantes :

sudo halt

sudo shutdown -r now

 

Mais nous cherchons un moyen de redémarrer le Raspberry sans devoir s'y connecter à distance.

 

Voila pourquoi je recherche une solution propre qui m'éviterait de devoir reformater sans cesse la SD.

 

Je vous remercie.

  • Sign in to reply
  • Cancel
Parents
  • gillou-tintin
    gillou-tintin over 8 years ago

    Bonjour,

    tu type ctrl + t puis reboot

    tu doit faire toujours toujours cette commande avant de faire une nouvelle installation ou tout autre modif  sudo apt-get update && sudo apt-get upgrade a la questiontu repond toutjours oui pour installer les nouvelles mise a jours.

    cordialement

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 8 years ago in reply to gillou-tintin

    My writing French is not that good. Do you mind if I try to help in English?

     

    So... The "reset" causes a brutal reset, only slightly less brutal than removing the power.

     

    I think that logging in to the console and typing commands is also not what you're looking for. You want a power button like on a PC that causes a shutdown.

     

    I would connect a pushbutton between GND and one of the GPIO ports. Then I'd write a script:

    #!/bin/sh

    pin=1 # better known as GPIO18, see the pinout documentations for the P1 connector on rasbperry pi.

    gpio mode $pin in

    gpio mode $pin up # I don't know if this obsoletes the above command, extra is easier than figuring that out.

    while [ `gpio read $pin` -eq 1 ] ; do

      sleep 0.1

    done

    halt

    call this script say "monpowerbutton" and save it in /usr/local/bin, change the mode to 755 and call it from /etc/rc.local:

    /usr/local/bin/monpowerbutton &

    That's it! A power button that causes a neat shutdown when pressed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 8 years ago in reply to gillou-tintin

    My writing French is not that good. Do you mind if I try to help in English?

     

    So... The "reset" causes a brutal reset, only slightly less brutal than removing the power.

     

    I think that logging in to the console and typing commands is also not what you're looking for. You want a power button like on a PC that causes a shutdown.

     

    I would connect a pushbutton between GND and one of the GPIO ports. Then I'd write a script:

    #!/bin/sh

    pin=1 # better known as GPIO18, see the pinout documentations for the P1 connector on rasbperry pi.

    gpio mode $pin in

    gpio mode $pin up # I don't know if this obsoletes the above command, extra is easier than figuring that out.

    while [ `gpio read $pin` -eq 1 ] ; do

      sleep 0.1

    done

    halt

    call this script say "monpowerbutton" and save it in /usr/local/bin, change the mode to 755 and call it from /etc/rc.local:

    /usr/local/bin/monpowerbutton &

    That's it! A power button that causes a neat shutdown when pressed.