Raspberry Pi Forum Not able to record audio from wolfson audio card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 674 subscribers
  • Views 735 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Not able to record audio from wolfson audio card

Former Member
Former Member over 11 years ago

Hi,

I am having raspberry model B and installed raspbian and applied the kernel patches as mentioned.

I am able to play any music file however, when it comes to record any audio either from headset/Line out the file is created but no audio.

Please help me out.

I am in urgent.

Thanks and Regards,

Sid

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 11 years ago

    siddarth mamidanna wrote:

     

    Hi,

    I am having raspberry model B and installed raspbian and applied the kernel patches as mentioned.

    I am able to play any music file however, when it comes to record any audio either from headset/Line out the file is created but no audio.

    Please help me out.

    I am in urgent.

    Thanks and Regards,

    Sid

    Hi Sid. Can you write down the stages you are going through to record so we can see? Perhaps you are missing a step

     

    imageimageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hi Matt,

    Thanks for your reply.

    I am following the below steps to perform audio recording:

    1. Plugged in 5 volts supply to wolfson audio card and 5 volts supply to raspberry pi
    2. Added patches to the kernel as directed.
    3. plugged in a headphone of into the headset.
    4. FYI I have attached the log file in which I had performed the steps.
    5. No output even after recording for atleast 1 minute.
    6. Also I tried to record a song from my mobile to headset using aux cable. but no output to lineout.

     

    It will be great help from your side if you resolve this issue. As I am stuck up in mid of my project

    Attachments:
    raspberry_audio.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago

    Hi Matt,

    Thanks for your reply.

    I am following the below steps to perform audio recording:

    1. Plugged in 5 volts supply to wolfson audio card and 5 volts supply to raspberry pi
    2. Added patches to the kernel as directed.
    3. plugged in a headphone of into the headset.
    4. FYI I have attached the log file in which I had performed the steps.
    5. No output even after recording for atleast 1 minute.
    6. Also
    Attachments:
    audio_record.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hi Matt,

    Thanks for your reply.

    I am following the below steps to perform audio recording:

    1. Plugged in 5 volts supply to wolfson audio card and 5 volts supply to raspberry pi
    2. Added patches to the kernel as directed.
    3. plugged in a headphone of into the headset.
    4. FYI I have attached the log file in which I had performed the steps.
    5. No output even after recording for atleast 1 minute.
    6. Also
    Attachments:
    0361.audio_record.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Well for one, if I remember from what I read from the documentation, adding the 5v supply to the Wolfson board is ONLY for powering the loudspeaker headers at the end of the board on the USB side.

     

    I too have been having some recording issues. I have managed to get some recording via the headphone jack but NOT the line-in via the audio editing program called "Audacity".

    I will say to get Audacity to pick up the 3 channel headphone Mic I had to change the device drop-down selection for the Mic selection to "snd_rpi_wsp: hw:(0,0): AIF:0" then I could record voice from my headset.

     

    Hope that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    I just made a discovery.

     

    The "Line In" port does NOT work with a Microphone. It is designed for Stereo sound input only, like from a male-to-male 3.5mm connector say from a iPod, Phone, or other device to the "red" LineIn interface. I don't know why I didn't realize it before. If you wish to record Mic audio, the headphone jack needs to be used. I'm not sure if you could put together a stereo 3.5mm jack for a Mic if that would work but it seems that the 3 channel headphone jack (Sound and Mic over 1 wire) needs to be used with a headset to record Mic input.

     

    Hope this helps anyone with the problem and hopefully saves them some time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    hi,

    Thanks for providing such a valuable information.

    After erasing the entire SDHC card and load the raspbian image to it and followed the instructions to patch the drivers to existing kernel.

    Now I am able to record from DMIC as well as Headphone and able to listen on Speakers/Line Out.

    Could any one give me a solution as in my project both my DMIC and speakers should be working together i.e. I had given the below command:

    $arecord -Dhw:0 -r 44100 -c 2 -f S32_LE | aplay -Dhw:0 -r 44100 -c 2 -f S32_LE

    but the issue is after few seconds a noise starts. (Here I am using DMIC for mic and speakers to listen)

    How to cancel the noise.

    Thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    The most obvious answer would be you're getting feedback - the mic is picking up the speaker output and it's going in a loop.  This makes a painful squeaking noise and you can often hear nothing else. 

     

    If not that then please can you try and describe what noise you're hearing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hi Joe,

    first of all sorry for replying so late.

    i am able to record and play with minimal noise.

    However, If I want to enable DSP firmware what are the prerequisites because as per the datasheet (WM5102) to enable AEC DSP firmware is required.

    Thanks in advance.

    Sid