Raspberry Pi Forum A lot of Playback items!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 685 subscribers
  • Views 3607 views
  • Users 0 members are here
  • wolfson
  • wolfson_pi
  • raspberry_pi
  • raspberrypi
  • raspeberry_pi_accessories
  • wolfson_microelectronics
Related

A lot of Playback items!

Former Member
Former Member over 11 years ago

I just entered alsamixer command to watch and change some volumes, but I found there is too many playback controls!

Why there is so many??

Is there something on the driver that create virtual devices or controls?

It's a little difficult to figure out which one is Line out

A list of the playback/recording controls could be helpful. I see some are for EQ, other controls i have no idea.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    This is the really short version...

     

    The card has three analog inputs:

    IN1R                  - Headset microphone. This is the right channel of analog input IN1. IN1L exists on the chip but isn't connected to anything.

    IN2L and IN2R    - The onboard DMIC microphones, left and right. Note that the markings on the board are wrong.

    IN3L and IN3R    - Line In, left and right.

     

    There are two analog outputs:

    HPOUT1L and HPOUT1R     - Headset, left and right.

    HPOUT2L and HPOUT2R     - Line Out, left and right.

     

    The card has three digital Audio InterFaces (AIF), each of which have a  receiver (RX) and a transmitter (TX).

    RX is signals coming in to the card from the Pi, the S/PDIF chip or the expansion connector. TX is signals going out from the card.

    AIF1     - Interfaces with the Raspberry.

    AIF2     - Interfaces with the S/PDIF chip.

    AIF3     - For future goodies. On the expansion connector.

     

    Speaker connections:

    SPKOUTL and SPKOUTR    - Onboard analog speaker circuit and amplifier.

    SPKDATL and SPKDATR    - Interface for Digital Speakers connected to the expansion connector.

     

    Then there is a gazillion of other stuff on the card, equalizers, filters, DSPs and whatnot.

    I'm working on writeup that will describe the card in more detail, but work and spending time with the family tends to get in the way. image

     

    At least I have managed to make an illustration...

    image

    Anyhow, I hope this clears some of the fog image

    --

    Ragnar

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Thanks! That clears the fog about all inputs!

     

    Now some detail got my attention: P1 pin 10 and P1 pin 8. Are those pins of RPi GPIO available for use? Or are they just for specific control? Are BCM chip or Board numbers?

     

    By the way, I use a Guitar Effects Processor software and JACK with default settings and worked well. I'm surprised because JACK also selected "Line in" as default image and didn't get confused with all those inputs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    They are connected to physical pins 8 and 10 on the Raspberry's 26-pin P1 header.

    GPIO14 and GPIO15 in the picture.

     

    They are normally used as the UART serial console, but that function is easy to disable.

    Raspberry Pi • View topic - Easily disable / enable serial console

    Raspberry Pi and the Serial Port

    With the serial console disabled, the two pins can be used as ordinary GPIO pins.

    GPIOs.png

    --

    Ragnar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    I guess I still able to use a serial lcd display, right? If I can, which options are available in the market?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    I guess I still able to use a serial lcd display, right? If I can, which options are available in the market?