OK, so I am trying to get images that I MAKE, meaning I OWN THEM, out of the RPi HDMI port, into a Video Switcher that has an HDSDI input only. And I have just spent about 18 hours trying to get an HDMI signal out of the RPi that the AJA will take. I am using an HDMI Splitter, which strips (amazingly) HDCP and the splitter is before the AJA to remove HDCP (which the AJA will not pass through) so I'm sure that is not the problem.
I have read this post http://www.raspberrypi.org/forums/viewtopic.php?t=5851
And this post 'config.txt' tag wiki - Raspberry Pi Stack Exchange
I've been all over the /boot/config.txt file trying all of the HDMI modes that I can find which are documented to be accepted by the AJA HA5 listed at this link https://www.aja.com/en/products/mini-converters/ha5#techspecs and I must have rebooted the RPi a hundred times trying different settings. But I have NOT ONCE gotten a signal out of the RPi that the AJA will recognize as an acceptable signal. I have 2 AJAs, 2 power supplies, good cables and I have tested the HDMI through the cables and units with another source (not the RPi) and it worked first time. But the RPi will not.
Also, the other output of the splitter goes to an LG HDMI TV which ALWAYS works, no matter what settings I try. I get different resolutions, overscans and underscans, etc, because I'm changing all the settings, but the AJA HA5 refuses to lock to the signal or pass it through no matter what the signal is.
This switcher cost a hell of a lot more than the RPi, and so did the AJA, so I am assuming I am using quality gear here.
Anyone have any idea how to get a working combination?
And can you set a new resolution attempt without having to reboot?