Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum LCD Hack - Is this possible?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 695 subscribers
  • Views 1299 views
  • Users 0 members are here
  • raspberry_pi
Related

LCD Hack - Is this possible?

Former Member
Former Member over 11 years ago

Hi guys

 

I have just salvaged this backlit LCD display (I beleive) from an old photo frame. Pictures are attatched, but it is a 761000937 E203460 display. The motherboard of the photoframe also contains an AUG375 (whic I believe is an SD/USB card reader) and also a Cheertek CT674-LF which I think is a display driver (I can't seem to find a datasheet for this).

 

My question: is it possible to connect this to the RPI/Arduino/Something? is there a driver board I can buy!!

 

 

Pictures: https://www.dropbox.com/sh/otztlhb3gzqtks0/AAAZKsa00bAPIx5xAp2yW9Xia?dl=0

 

Thanks Guys!!

 

Tom

  • Sign in to reply
  • Cancel
Parents
  • bodgy
    bodgy over 11 years ago

    Judging by the number of pins I would guess that this display is one that uses LVDS and checking out similar ones on Alibaba (10.1 Inch Tablet Display H-101d-1ba 73002001242c E203460 235x143mm Thinckness 4mm 60pin - Buy Tablet Lcd Display,Display…)

     

    What I think you might be looking for is something along the lines of these, it will be cheaper than making one yourself.

     

    Store | Chalkboard Electronics

     

    http://www.embest-tech.com/product/modules-for-raspberry-pi/fhd8000-lr.html

     

    Colin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to bodgy

    And also Tom, bear in mind that wiring up from that flat-flex to the board is not easy, and you'll also likely need a DC-DC converter to supply the voltage for the LED or CCFL backlight.

    A fair bit of effort basically.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to bodgy

    And also Tom, bear in mind that wiring up from that flat-flex to the board is not easy, and you'll also likely need a DC-DC converter to supply the voltage for the LED or CCFL backlight.

    A fair bit of effort basically.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    yes the voltages could very well be all over the place  I would measure the voltages still in the original device if you can then scope out the video signals  to get  an idea of what you can do with it.

     

    Bear in mind that a LCD with composite video input is about £10 from EBAY as a reversing Camera system!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to Problemchild

    I have a "new" display that I wanted to connect to my 'pi. So I have a full datasheet. I need three voltage supplies: something like -10V, +11V and +19V. Mind you: that's very approximate the specs state something like betwee 10.2 and 10.6. Oh, and for the backlight we needed a current source at something between 10 and 20V. So you'd go wrong if you assume it is a voltage that you measure at currently 17V... It can be 16V tomorrow when the weather is hotter....

    • Cancel
    • Vote Up 0 Vote Down