Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum mmc0: Timeout - Help? No SD card reader!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 677 subscribers
  • Views 1137 views
  • Users 0 members are here
  • raspberry_pi
Related

mmc0: Timeout - Help? No SD card reader!

Former Member
Former Member over 11 years ago

Hey. I installed Raspbian on my Pi a few months back, but of course it broke down (happens to me a lot).

 

Now I get a mmc0: Timeout waiting for hardware interrupt - cmd13 OR cmd12

I do not have an SD card reader, so I can't put a new OS on it, so what can I do? Is it possible to do it through USB through the Pi? Or hook up to WiFi using the dongle, then download the file and burn it on the SD card?

 

Any help would be appreciated. Thanks! image

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    There are a number of possibilities.  One is that the SD card has gone bad, in which case you need to rewrite the OS image to your existing SD card or to a new one.  Either way you need an SD card reader as Mike has said.  Another is that the SD card socket is making poor contact.  There's an item about this at the RasPi Troubleshooting Wiki: http://elinux.org/R-Pi_Troubleshooting#Pi_boots_sometimes_but_not_always  The SD card socket has very fragile pins, so be careful.

     

    The easiest way to screw up an SD card is to turn off RasPi power without doing a "shutdown" first to flush the disk cache.  The GNU command is "sudo shutdown -h now".  GUIs usually have a shutdown command you can click somewhere.

     

    Mike is correct that the only way to boot RasPi is from a working SD card.  Once the boot process is underway it's possible to mount other drives, but I've never done it.  RasPi always starts with the SD card.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to johnbeetem

    As a non-typical configuration, I have some of my 'PIs boot from the SD and then work from NFS. So, once they are booted, I have the raspberry pi capable of removing the SD card while it is on and then inserting a new SD card to either read or write.

    However this does require a working boot-NFS SD card, as wel as the setup with the server for DHCP and NFS-root.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 11 years ago in reply to johnbeetem

    As a non-typical configuration, I have some of my 'PIs boot from the SD and then work from NFS. So, once they are booted, I have the raspberry pi capable of removing the SD card while it is on and then inserting a new SD card to either read or write.

    However this does require a working boot-NFS SD card, as wel as the setup with the server for DHCP and NFS-root.

    • Cancel
    • Vote Up +2 Vote Down