Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Top 5 Reasons The Raspberry Pi Sucks
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 710 subscribers
  • Views 5951 views
  • Users 0 members are here
  • raspberry-pi
  • raspberrypi
Related

Top 5 Reasons The Raspberry Pi Sucks

gadget.iom
gadget.iom over 11 years ago

Stumbled upon this article. Wise words of caution. image

 

Top 5 Reasons The Raspberry Pi Sucks | Raspberry Pi Spy

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    Very amusing satire.  However, it is worthwhile to point out that even though RasPi Model A/B is "the size of a credit card" it won't fit in an Altoids box because it doesn't have rounded corners like a credit card.  The BeagleBone does.  Gerald Coley told me those rounded corners and mounting holes made BeagleBone placement and routing a real pain.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to johnbeetem

    I might have to try one of these beaglebone devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to gadget.iom

    The BBB is very well put together I like the fact you can use a battery to power it which is great for mobile devices!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to Problemchild

    Problemchild, Would you recommend the BeagleBone Black edition?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to gadget.iom

    I liked it  Shabaz is the expert on that device ...see what he's done with it !

     

    I think the real time aspect with the PRUs is cool as well more speed is good as well.

     

    My ODROID C has arrived I should do a quick blog on it latter

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    That was quick, looking forward to hearing about the Odroid!

    I saw some initial review but most of it focussed on HDMI, which isn't something that I would use that board for personally, but probably others have different projects that need this. I'd rather see information on CPU performance, peripherals and interfaces!!

     

    Hi Paul,

    The BBB is a nice product. It's one of the best single-board computers for portable projects because of the in-built battery charging that John mentioned, and good performance (probably twice as fast on average as RPI for programs using the main CPU), and very high throughput (around 1Gbps) if you want to feed data to/from the board. The PRUs that John mentions are additional built-in processors that can be programmed in C or assembler, and they function at 200MHz and allow for I/O to operate at this rate too (which is very unusual for processors).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    That was quick, looking forward to hearing about the Odroid!

    I saw some initial review but most of it focussed on HDMI, which isn't something that I would use that board for personally, but probably others have different projects that need this. I'd rather see information on CPU performance, peripherals and interfaces!!

     

    Hi Paul,

    The BBB is a nice product. It's one of the best single-board computers for portable projects because of the in-built battery charging that John mentioned, and good performance (probably twice as fast on average as RPI for programs using the main CPU), and very high throughput (around 1Gbps) if you want to feed data to/from the board. The PRUs that John mentions are additional built-in processors that can be programmed in C or assembler, and they function at 200MHz and allow for I/O to operate at this rate too (which is very unusual for processors).