Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Power DC Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 711 subscribers
  • Views 4463 views
  • Users 0 members are here
  • eagle
  • eaglecad
  • raspberry-pi
  • raspberrypi
  • schematic
  • power
Related

Raspberry Power DC Power Supply

gadget.iom
gadget.iom over 11 years ago

A recent discussion by Robin Gunning (Raspberry pi powersupply change from micro usb to dc power plug) led me to investigate the feasibility of creating a board allowing a DC power jack to be connected to the Raspberry Pi.

 

 

I have created my first ever Eagle Schematic but would appreciate some feedback on the suitability of the design and any comments/suggestions you may have for improvements or potential pitfalls.

 

image

The aim is to have a 26-way extension header so that shields can be added on top of this board. The 26-way header should also be compatible with the 40-way header on the newer plus editions of the Raspberry Pi.

 

Thanks

Paul

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Paul,

     

    Your design on its own looks fine (just an EAGLE thing, if you use the 'Net' icon instead of the 'Wire' icon to draw your wires, then it will automatically add blobs at junctions; the 'wire' icon need  never be used in a schematic, although it works electrically just like the Net icon) and will definitely function. But looks like you've got to grips with EAGLE quickly overall.

     

    The only concerns are (1) If you use a (say) 9V DC supply, then around 2W of power is dissipated if the RPI consumes 5V 500mA since (9-5) * 0.5 = 2W (the RPI may use less power, the 500mA was a guess). 2W is a enough to get a small heatsink hot : (

    and (2) lack of schematics for the RPI B+ make me uncomfortable wiring to the pins like this, although in theory it should be fine

    and (3) might be worth double-checking the pinout of the 7805, most models have pin 2 as the ground, not pin 3, but I wasn't sure which package you were using, so it may be fine.

     

    So to summarize, (assuming the pinout of the 7805 is correct) in practice this board would probably be fine, as long as a (say) 7V supply was used (although that may be borderline for a 7805) or with a heatsink.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to shabaz

    Well... > say 8V input would require a heatsink. And the current that the raspberry pulls would require > 8V to allow for the dropout of the 7805. (Datasheets usually claim about 2V, but that's "typical at 25C", while calculating the worst-case situation you quickly go towards the "rule-of-thumb" that 3V is required).

     

    I have 5V powersupplies with that plug. So I was thinking of simply "dropping the regulator". On the other hand, adding a simple-switching powersupply would also be "nice".

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to rew

    I agree with all you mention. I too have plenty of supplies that are 5V with that plug. That might be a better board Paul, nice and simple - just a DC socket and the connector for the RPI.

    The other option Roger mentions would be pretty cool too, especially if it could handle automotive supply, and had some latching Molex connector or something as well as the DC socket you already have. But then it is a more complex circuit although probably there are some off-the-shelf DC-DC converters that could be soldered on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to rew

    Thanks Rodger.

    Will look into switching powers supplies too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 11 years ago in reply to rew

    Thanks Rodger.

    Will look into switching powers supplies too.