Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Power DC Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 711 subscribers
  • Views 4480 views
  • Users 0 members are here
  • eagle
  • eaglecad
  • raspberry-pi
  • raspberrypi
  • schematic
  • power
Related

Raspberry Power DC Power Supply

gadget.iom
gadget.iom over 11 years ago

A recent discussion by Robin Gunning (Raspberry pi powersupply change from micro usb to dc power plug) led me to investigate the feasibility of creating a board allowing a DC power jack to be connected to the Raspberry Pi.

 

 

I have created my first ever Eagle Schematic but would appreciate some feedback on the suitability of the design and any comments/suggestions you may have for improvements or potential pitfalls.

 

image

The aim is to have a 26-way extension header so that shields can be added on top of this board. The 26-way header should also be compatible with the 40-way header on the newer plus editions of the Raspberry Pi.

 

Thanks

Paul

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    If you are really into bread boarding the power supply, I've had good luck with these tiny switched regulators (http://www.pololu.com/category/131/step-down-voltage-regulators).  I mount them onto the bread board when prototyping, or solder onto the circuit board when the design is complete.  I can hardly build one from scratch for the price of these switched power supplies on a breakout.  Also  note, that the input voltage on these is quite high, allowing for use from a car electrical system with all it's over voltages.  There are also step up and step up/down which are great for battery use.  Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    If you are really into bread boarding the power supply, I've had good luck with these tiny switched regulators (http://www.pololu.com/category/131/step-down-voltage-regulators).  I mount them onto the bread board when prototyping, or solder onto the circuit board when the design is complete.  I can hardly build one from scratch for the price of these switched power supplies on a breakout.  Also  note, that the input voltage on these is quite high, allowing for use from a car electrical system with all it's over voltages.  There are also step up and step up/down which are great for battery use.  Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    Thank you for that!

    Will give some of those a try. Hoping to find a supplier here in the UK as delivery costs more than the modules themselves image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to gadget.iom

    If you are in the UK you can easily get the 5V 2-4A supplies  that CPC do:

    http://cpc.farnell.com/ideal-power/25hk-ab-050a400-d5-1/psu-desktop-5v-4a-3-pin-iec/dp/PW03335?in_merch=Products%20From%20This%20Range&MER=e-bb45-00001003

    image

    £9.23 less on a bargain day and will power your Pi all day with what ever extra bits you throw at it and no additional regulators required ...Simples!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • srinivasansmv
    srinivasansmv over 11 years ago in reply to Problemchild

    thank you nice answer