Raspberry Pi Forum Battery Question, will I burn my face off?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 687 subscribers
  • Views 1830 views
  • Users 0 members are here
  • raspberry_pi
Related

Battery Question, will I burn my face off?

larisbird
larisbird over 11 years ago
I'm trying to expand capacity for a Duracell power bank (3.7v 2600 mAh) so I can power my portable RasPi project with it.  I've taken a battery (3.7v 2800 mAH) from a cheap tablet and I'm wondering if I just connect the negative of the Duracell to the positive of the Tablet battery then take the negative of the Tablet battery and connect it back to the board of the Duracell power bank, if it will increase the capacity of the power bank and function normally or will it blow up in my face melting it Raiders of Lost Ark style?
I'm a novice hobbyist and any pointers would be a huge help.
A little more detail about my project: I'm installing a RasPi with RetroPie into an Original Gameboy case for a pretty cool emulator.  I've found a step up chip to power the new display but have run into the issue of portable power.  I'd like a little more capacity than the batteries that I've seen Ben Heck and others use.
Thanks for your time and I hope to hear from anyone
Attachments:
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    Problemchild over 11 years ago

    The flat battery looks like a LIPO and the round one a conventional Li-Ion. As the others as said it's best not to mix the different chemistries  together.

    Also  the charger inside the powerbank is expecting to charge a 3.7v nominal device so you will need to put two batteries of the same type in parallel (not series) also because you are effectively making 1 cell from 2 or more you need to have cells which are more or less matched in spec so that they charge and discharge in similar ways as you have no way of balancing them individually( you can get these from suppliers already made up!).

     

    Your current power bank should power the RPI for 3-5 hours I think if you need much more then you really need a bigger bank  an alternative may be a simple 12V Gel Cell and 5V regulator. I would expect 10 hours from a 5AH  cell  atleast depending on the regulator type usage etc.

     

    Thanks for sending  the pictures BTW as this makes helping you much easier. It's this kind of thing that gets your questions answered in the best way possible .

     

    What is the end purpose of your project?

     

    Good luck !

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 11 years ago in reply to Problemchild

    People are making more of a fuss about connecting different batteries together than is necessary.

     

    For starting a boeing 787 you absolutely need balanced cells of the same chemistry: You're charging them close-to-max, you're discharging them at max when you really need them.

     

    But for hobby purposes where you're adding an extra battery to have a larger capacity, this is less of an issue.

     

    Worst case, what will happen is that one battery will drain from "almost full" to "almost empty" between 3.8 and 3.7V. And that the other will do so between 3.7 and 3.6V. Then during discharge you'll be (mostly) running on just one battery when the voltage is between 3.7 and 3.8, so you'll have to respect the "max discharge" for that battery (and later on in the discharge for the other). Similarly, during charge, you'll have to stick to the "max charge" of the slowest battery.

     

    On the other hand, being extra cautious is a good idea too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 11 years ago in reply to Problemchild

    People are making more of a fuss about connecting different batteries together than is necessary.

     

    For starting a boeing 787 you absolutely need balanced cells of the same chemistry: You're charging them close-to-max, you're discharging them at max when you really need them.

     

    But for hobby purposes where you're adding an extra battery to have a larger capacity, this is less of an issue.

     

    Worst case, what will happen is that one battery will drain from "almost full" to "almost empty" between 3.8 and 3.7V. And that the other will do so between 3.7 and 3.6V. Then during discharge you'll be (mostly) running on just one battery when the voltage is between 3.7 and 3.8, so you'll have to respect the "max discharge" for that battery (and later on in the discharge for the other). Similarly, during charge, you'll have to stick to the "max charge" of the slowest battery.

     

    On the other hand, being extra cautious is a good idea too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Problemchild
    Problemchild over 11 years ago in reply to rew

    Um since my 10Ah power pack was only like £15  and you can get matched cell batteries quite easily I wouldn't even bother taking the risk of mixed chemistries.. Should be OK but since he'll probably be having it unattended then he may as well do it properly!