Raspberry Pi Forum Battery Question, will I burn my face off?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 687 subscribers
  • Views 1848 views
  • Users 0 members are here
  • raspberry_pi
Related

Battery Question, will I burn my face off?

larisbird
larisbird over 11 years ago
I'm trying to expand capacity for a Duracell power bank (3.7v 2600 mAh) so I can power my portable RasPi project with it.  I've taken a battery (3.7v 2800 mAH) from a cheap tablet and I'm wondering if I just connect the negative of the Duracell to the positive of the Tablet battery then take the negative of the Tablet battery and connect it back to the board of the Duracell power bank, if it will increase the capacity of the power bank and function normally or will it blow up in my face melting it Raiders of Lost Ark style?
I'm a novice hobbyist and any pointers would be a huge help.
A little more detail about my project: I'm installing a RasPi with RetroPie into an Original Gameboy case for a pretty cool emulator.  I've found a step up chip to power the new display but have run into the issue of portable power.  I'd like a little more capacity than the batteries that I've seen Ben Heck and others use.
Thanks for your time and I hope to hear from anyone
Attachments:
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    Problemchild over 11 years ago

    Um if you are using a 12V screen then use  a standard gel battery or better still on of those Lithium packs that come with a charger from EBAY or the likes . They are light for mobile applications give you a nice power level and cheap enough you will need to use a small switch mode module for the 5V output.You should be safe on assuming 85% efficiency in what ever calcs' you are doing !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 11 years ago

    Um if you are using a 12V screen then use  a standard gel battery or better still on of those Lithium packs that come with a charger from EBAY or the likes . They are light for mobile applications give you a nice power level and cheap enough you will need to use a small switch mode module for the 5V output.You should be safe on assuming 85% efficiency in what ever calcs' you are doing !