I saw a link online that converted the display to accept 5v for power. However, the board for my display is not the same as the examples in the thread (apparently there are many different boards while the exterior looks the same).
What are your thoughts on attempting to modify the board so the display could be powered with 5 volts?
Um if you are using a 12V screen then use a standard gel battery or better still on of those Lithium packs that come with a charger from EBAY or the likes . They are light for mobile applications give you a nice power level and cheap enough you will need to use a small switch mode module for the 5V output.You should be safe on assuming 85% efficiency in what ever calcs' you are doing !
Jack Norman wrote:
What are your thoughts on attempting to modify the board so the display could be powered with 5 volts?
I'd say if you have the knowledge to do it yourself, go ahead and do it. (i.e. if you're asking: don't)
If you don't have exactly the same screen, figuring out how to do it, probably involves some "trouble shooting" which is difficult if you don't have the appropriate skillset (and tools!).
I really appreciate all the help!!
I'm sure I have the tools, it shouldn't take more than a mulitmeter and some patience right? If we're talking oscilloscope and the like, then I'll probably go a different route.
Now this would probably be outside my skillset but one of the main reasons for doing these types of projects is to learn new skills!
So, any advice on how to do that would be greatly appreciated but if it's too complicated to explain then I understand completely!
Again, thank you so much for the replies and I hope you have a fantastic New Year.
it shouldn't take more than a mulitmeter and some patience right?
Actually less than that ..... observation.
You should be able to identify a regulator, or failing that a transistor and zener.
The IC's they use (assuming they have a label) will have a datasheet that specifies the supply pins and the voltage.
You can then trace back to find the regulator, if its not obvious.
These clues are the first thing I would look for, then work backwards to see they don't have anything user higher than 5v.
Mark
Jack your post motivated me to do a real live test on a RPI model B and a battery pack I had.
Hope you'll find it useful