Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum microphones and the cirrus audio card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 708 subscribers
  • Views 3970 views
  • Users 0 members are here
  • wolfson
  • cirrus
  • recording
  • raspberry_pi
  • raspeberry_pi_accessories
  • microphones
Related

microphones and the cirrus audio card

soundcamp
soundcamp over 11 years ago

I want to use stereo electret condenser microphones with this card. They need a a bias voltage (Plug in Power) of around 5V.

 

The Wolfson only included mono microphone support through the Mic in plug.

 

The comparison table for the Cirrus says it supports stereo microphones through the Line in, and the video introduction to the card mentions that bias voltage is provided for electret condenser microphones, but doesn't give more detail.

 

It would be great to have confirmation of what exactly this card provides in this direction.

 

This is important because it decides if the card enables the Pi to be used as a high quality audio recorder without an additional soundcard - as the Wolfson sadly could not.

 

Thanks

 

Grant (soundCamp)

  • Sign in to reply
  • Cancel
Parents
  • timg73
    timg73 over 11 years ago

    There is definitely a microphone bias circuit in the schematics, and even a script to enable recording from a biased microphone.  But I tried just now and couldn't actually measure any bias voltage.on the line-in connector.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • soundcamp
    soundcamp over 11 years ago in reply to timg73

    Ok Great - thanks Tim

     

    so maybe it has to be enabled?

     

    bw

    grant

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 11 years ago in reply to soundcamp

    Hi Grant,

     

    Thank you for your hard work, and to the others who are working on this cirrus logic audio card too.

     

    I've tried the new image, it works, I've managed to stream on the test stream, there's a little interference coming through a "buzzz" which changes as you move the card and wires about, you can get it so that it is almost gone too.

     

    Not sure if it has to get to the GUI? Would have liked headless, I've tried turning off the GUI but it's got some script running for the IP which stalls the command line. Changing the host name breaks some things too.

     

    I'm confused as how darkice works without Icecast2.

     

    My new account for the testing microphone site breaks the streaming as well, not sure why, there is a conflict of terms in the conf file to the information given after new account conformations.. being a fair newbie probably isn't helping me comprehend what is going on in that config file.

     

    Was hoping to run SAMBA, WEB Server, noip ddns client, sakis3g, Icecast2 and stream to another online server, though I am quite interested with the microphone radio site, as it works on "switch on", so why not use this without me faffing about trying to get other things to work when not needed? probably the challenge! but an easy excuse not to try.

     

    I hope to have some answers from the help guys on the microphone site, so with luck will have "Liverpool_3D_binaural" sound stream up and running soon.

     

    I am so grateful for those who have worked hard to get things going, thank you very much guys!

     

    Regards

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • soundcamp
    soundcamp over 11 years ago in reply to binauralhead

    Hi Alan and all

    I'm glad the disk image has been useful to get started. I will check how to disable the automatic darkice script to make it easier to work with.

     

    I'm sorry that realistically I won't be able to provide much detailed advice and support on applying the card to other uses - although I am happy if it is contributes to those.

     

    I should also be clear about some limits to its use:

     

    This disk image is designed specifically as an approach for live audio streaming to the Locus Sonus open microphone soundmap.

    The notes etc on the soundCamp resources page are also aimed at that.

    The soundmap itself is a specific project, with specific parameters, described here http://locusonus.org/ -Locustream

    It's a long standing project (not mine), and isn't intended to include eg conventional radio material, recordings, musical performance, etc


    So if people are experimenting with the disk image, beyond preliminary testing, you should alter the stream configuration file to point at your own icecast server (which you could also set up on a local machine).


    Please use the disk image for your own projects as useful.


    But please don't use the Locus Sonus server for general experimentation.

     

    I should have been clearer about that when I shared the link.

     

    Thanks

    Best wishes

    Grant

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 11 years ago in reply to soundcamp

    Hello Grant, et al..

     

    The thought of "this could get interesting" came to mind when I realised that with a fresh image, network connection and power on, you would be streaming, if it were to be popular to download ...... When I realised this, I was very conscious of being switched on, and on-line - hence my swift move.

     

    "The soundmap itself is a specific project, with specific parameters, described here http://locusonus.org/ -Locustream

    It's a long standing project (not mine), and isn't intended to include eg conventional radio material, recordings, musical performance, etc"


    This sounds like the perfect place for my binaural microphones!! This is very much NOT a conventional way to record things or to have streaming live, and is something I have been looking for many months. If anyone cares to have a listen to any of my binaural recordings, and see what "Frank the terrorist" has been upto please wear your best headphones and click here: https://soundcloud.com/binauralhead you can also see what I have been up to on the blog, address is on the soundcloud channel, if you read the full profile on "Frank".


    Having the raspberry Pi in a bag (or anywhere), with battery and 3G/4G dongle and a "binaural microphone" .. would, for me, be quite something, esp if there was a dedicated website that had many binaural microphones placed about the globe, to experience being there would be totally awesome. Unless you have experienced listening with headphones what binaural audio is, you will have no idea what I am on about.


    If it were not for people like Grant, and the people who are doing the microphone project, I would not be so excited with this idea, and it would probably never have happened for me. In the last 12 months of being interested with binaural audio I have met, quite by chance, some very famous people, and been to famous film studios with both my dummy head microphones - all were totally awesome experiences!!


    Being able to listen to an audio stream that has very good quality, live (or recorded) from your iPhone, MAC or PC, Library or on-line radio station is just as good, if not better than 3D vision! and if combined...


    I feel that something very good could come of this, and if not, it's something that keeps me interested with sound, the raspberry pi, and new people to talk with, who could want for anything more?


    Slice of Pi anyone?


    Regards

    Alan


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • soundcamp
    soundcamp over 11 years ago in reply to binauralhead

    Hi Alan

    This all sounds good. It's great we're on the same wavelength.

    Happy to discuss more about live streaming, maybe off- list - we may be straying from the theme..

     

    BTW if you're working with the image, you can disable the auto streaming darkice feature by renaming the file:

     

    Desktop/stream_settings/run_on_boot/start_stream.sh

     

    to something else.

     

    bw

    grant (soundtent.org)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to soundcamp

    These big images are a waste of time in my opinion. The only thing you need is a kernel (with realtime capabilities) Here is 3.12.33 for the os of YOUR choice.

    https://blog.georgmill.de/2015/02/18/update-for-wolfson-audio-card-on-raspberry-pi/

     

    Have fun :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to soundcamp

    Hi Grant,

     

    Did this mic, Primo EM-172 , work?

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 11 years ago in reply to soundcamp

    Hi Grant -- et al

     

    Just a quick message on here if others have been following the thread.

     

    Up and running (at present) with the Cirrus Logic audio card here: Lan2Lan.no-ip.com (images & info).

    link to audio stream here: http://locus.creacast.com:9001/liverpool_ormskirk

     

    Thank you to those who made this real for me.

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to binauralhead

    Hey, there are only birds to hear? What kinda channel is this? ;-))

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 11 years ago in reply to e14 Contributor

    This is binaural audio - only ever realised when the listener wears headphones.

    Bad weather out there just now, but you should be able to tell what is above you and below the head, lots of things happen in this garden, but not all of the time. On test at present, testing the cirrus logic card. Aircraft sound interesting image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to binauralhead

    With a dummy head? Or are u using the mics on the audio card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to binauralhead

    With a dummy head? Or are u using the mics on the audio card?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • binauralhead
    binauralhead over 11 years ago in reply to e14 Contributor

    With a home made dummy head (with external mics going through the line in on the card) - see Lan2Lan.no-ip.com for images and more info - it's an on going project, this one uses 3D printed ears of my own ears, their not quite a realistic plaster cast of them, but I have a set of those as well.

     

    I've now managed to replace one of the mics on the dummy head in the garden and set the levels correctly.

     

    Noise levels on the cirrus logic audio card seem excellent, as I can't seem to hear any through the line in socket. I've not tried the built in mics, or used any other features, just the line in

     

    Regards

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to binauralhead

    Cool project. Sounds very interesting.

    Regards

    Georg