Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 - does it hit the mark?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 713 subscribers
  • Views 7234 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 - does it hit the mark?

tekmeister
tekmeister over 11 years ago

While previous articles had the release slated for 2017, it seems the next-gen Raspberry Pi is being released today:

 

http://www.theregister.co.uk/2015/02/02/raspberry_pi_model_2/

 

Pi v2 will come with a quad-core 900MHz processor and 1GB RAM (an upgrade from the single-core 700MHz and 512MB RAM of the original). Also the price will be the same ($35). It looks like the footprint is the same as the B+.

 

As I mentioned in November How to make a better Pi, the two main things in the Pi's favour are cost and community, but I have run into a number of limitations with the original Pi. I'm hoping this new version addresses most of them, but time will tell, as full details aren't available yet.

 

Aside: I'm wondering if this is what the upcoming "Enchanted Objects" challenge is about.

  • Sign in to reply
  • Cancel
  • mconners
    mconners over 11 years ago

    Honestly I'm pretty excited that Raspberry Pi is now available in a quad core package. Plus with the new SOC I might actually be able to run Ubuntu on it. I wouldn't mind trying one out.

     

    The competition between vendors should ultimately benefit us, the consumer, in the long run. The Ras Pi drove down the price of the BBB, or so it seems, maybe the odroid C1 forced the RPF to accelerate their plans to upgrade. I don't know for sure. But it seems like I had seen some press releases that said nothing significant was planned for a couple of more years.

     

    Who knows what will come next, but chances are we won't be able to afford to keep up with all the advances.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    I like the ODROID-C1 (I have one) but at this time there are a few problems with them:

     

    1.  No documents on the ARM SOC. In one of the wiki threads it said it was going to be released Jan. 15 but I have been back several times since then and I am still waiting.

     

    AmS805 data sheet link is on this page: http://hardkernel.com/main/products/prdt_info.php?g_code=G141578608433&tab_idx=2

    2.  No documents on the GPU, and there is not likely to be any in the future because it is not their IP.

    It's a MALI GPU.  There's an open-source project called LIMA that's trying to produce open-source documentation and drivers.  I don't know how far they've gotten.  I'm delighted that RasPi opened up the VideoCore 4 last year and hope that starts a trend toward open documentation.  I've read that it's mostly USA patent law that preventing Progress in Science and Useful Arts in the GPU arena.

    As I have said several times in Raspberry Pi forums schematics are all I really need to find most problems so I have no problem with this as long as the schematics are accurate.

     

         There are a couple of problems with the current ODROID-C1 schematics however. There are two page 21s and two page 22s, both sets are for the USB1 - USB4 circuits. Both are related to the same issue, copying pages where the schematic is virtually the same, but not changing the signal net/bus names. All the nets/buses are labeled USB1 and USB2 on both pages so it is difficult to tell which is 1/2 and which is 3/4. There are different reference designators on the pages using A/B to differentiate between them which is carried over to the PCB silk screen so by it can determined which is which on the schematic, it's just better to have accurate schematics to start with.

    We're still waiting for the RasPi B+ schematics.  The RasPi page only has a single-pager with interfaces: http://www.raspberrypi.org/documentation/hardware/raspberrypi/schematics/

     

    There's no A+ schematic at all.  Who knows when the RasPi 2 schematics will be released.  It took a long time for the RasPi Model A/B schematics to come out.

     

    The ODROID schematics are a bit hard to follow since they're hierarchical instead of flat.  There is only one page 21 and one page 22 in the design, but the printout has two instances of each with different component names.  You have to go back to the root schematic on page 1 to make sense of it and see how the signal names map.  It's a pain: I far prefer flat schematics for a board this size, but schematic styles vary.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nlarson
    nlarson over 11 years ago in reply to mcb1

    Hi Mark - if you are having a hard time finding the product on New Zealand's site - try this link here: http://nz.element14.com/raspberry-pi/raspberrypi-2-modb-1gb/sbc-raspberry-pi-2-model-b-1gb/dp/2461030?ost=2461030

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to nlarson

    Nicole

    Thanks very much

    Someone gave a link to the design centre, and that gave me an inside to be able to order it.

     

    I note the numbers have dropped since I first ordered ....

     

    The one good thing about element14 is the product code number stays constant (well except for MCM) ....

    Thanks

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to mconners

    Michael Conners wrote:

     

    The competition between vendors should ultimately benefit us, the consumer, in the long run. The Ras Pi drove down the price of the BBB, or so it seems, maybe the ODROID-C1 forced the RPF to accelerate their plans to upgrade. I don't know for sure. But it seems like I had seen some press releases that said nothing significant was planned for a couple of more years.

    It's in the RasPi FAQs: http://www.raspberrypi.org/help/faqs/#generalFuture

    As of the July of 2014, an updated version of the Model B, the Model B+, has been released.  Beyond this revision... there are no immediate plans for the next model;  a new model may be released in 2-3 years, but this is not a firm schedule.

    I can only guess that RasPi is as surprised by the RasPi 2 as we are image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 11 years ago in reply to johnbeetem

    I literally laughed out loud. Good one, John. And thanks for the reference, I knew I'd read it somewhere.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago

    Did I miss something or is there still no way to handle analog easily without an addon?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to michaelwylie

    Michael Wylie wrote:

     

    Did I miss something or is there still no way to handle analog easily without an add-on?

    From what I've read, the RasPi 2 is the same as the RasPi model B+ except for the quad core CPU and 1GB DRAM.  Everything else is the same, so no analog without and add-on.  ODROID-C1 has analog inputs image  ADC on the Odroid

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tekmeister
    tekmeister over 11 years ago in reply to johnbeetem

    Yes it looks like the peripheral set for v2 is the same as for the original. The decision was probably made for compatibility reasons, but it's disappointing to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 11 years ago in reply to mconners

    Thanks Mike (and John) !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>