Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 - does it hit the mark?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 713 subscribers
  • Views 7245 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 - does it hit the mark?

tekmeister
tekmeister over 11 years ago

While previous articles had the release slated for 2017, it seems the next-gen Raspberry Pi is being released today:

 

http://www.theregister.co.uk/2015/02/02/raspberry_pi_model_2/

 

Pi v2 will come with a quad-core 900MHz processor and 1GB RAM (an upgrade from the single-core 700MHz and 512MB RAM of the original). Also the price will be the same ($35). It looks like the footprint is the same as the B+.

 

As I mentioned in November How to make a better Pi, the two main things in the Pi's favour are cost and community, but I have run into a number of limitations with the original Pi. I'm hoping this new version addresses most of them, but time will tell, as full details aren't available yet.

 

Aside: I'm wondering if this is what the upcoming "Enchanted Objects" challenge is about.

  • Sign in to reply
  • Cancel
  • gdstew
    gdstew over 11 years ago in reply to johnbeetem

    "It's a MALI GPU.  There's an open-source project called LIMA that's trying to produce open-source documentation and drivers.  I don't know how far they've gotten.  I'm delighted that RasPi opened up the VideoCore 4 last year and hope that starts a trend toward open documentation.  I've read that it's mostly USA patent law that preventing Progress in Science and Useful Arts in the GPU arena."

     

    Yes I am aware of this project and trying is exactly the right way to put it. GPUs are very complicated devices and open documentation is really the only way to get it right . Like you I hope the others follow suit however I would not hold my breath,

    there have been rumors but they are at least a couple of years old now and nothing has changed.

     

     

    "We're still waiting for the RasPi B+ schematics.  The RasPi page only has a single-pager with interfaces:"

     

    Yes I know, I have brought up my displeasure with this several times in these forums. As far as I can tell the one page details all of the changes made between the B and B+ EXCEPT the new USB IC  and USB interface circuits. I have no idea why they

    have suddenly gotten secretive about this and it does not sit well with me that they have. Plus my attempts to get this changed have to date been ignored. I may wait until the schematics are(?) published before buying a Pi 2.

     

     

    "The ODROID schematics are a bit hard to follow since they're hierarchical instead of flat.  There is only one page 21 and one page 22 in the design, but the printout has two instances of each with different component names.  You have to go back to the root schematic

    on page 1 to make sense of it and see how the signal names map.  It's a pain: I far prefer flat schematics for a board this size, but schematic styles vary."

     

    My explanation pretty much describes exactly what they are. The part of page one you describe is just a block description that does not give any details that are useful when trying to trace a problem back to the source (pins). Not differentiating

    between which circuits on the schematics are for USB ports 1/2 and which are for USB ports 3/4 is just not the right "style" period. In my 30+ years in electronics I have never seen another schematic (other than maybe a bad preliminary one) that

    used this "style".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • markvenn
    markvenn over 11 years ago in reply to bodgy

    I agree about win 10 support. A free version I understand, will they admit that very few people are going to have touch screens for the Pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to tekmeister

    The main disappointment for me is that it still seems to use the same brain dead Ethernet via SMC usb chip arrangement. And of course the Ethernet is only 10/100.

     

    Withe the better processor they really should have managed 1G Ethernet and some kind of high speed low latency IO port (PCIE would be ideal but even proprietary would be an advance.)

     

    The PI is still terribly limited by lack of general purpose IO with performance to match the processor.

     

    Despite these gripes the big plus is the possibility of Windows - now if Microsoft could only bring themselves to munch a tiny bit of humble pie and offer VB6 (or better still VB7  - ie VB6 updated but NOT vb.net) on it - then you would have a 21st century computer that anyone could code.

    And while I'm on a rant roll - I can run a VB6 exe (ie binary file) on Windows2k, XP, Vista, 7 and 8 (and 10 promised)  - spanning 15+ years of OS offerings - try that on Linux ! (substitute any language you like for VB6).

     

    (BTW I know that the RPi can't be binary compatible with VB6 on windows)

     

    (Way off thread here  - can't think what was in the breakfast coffee.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to gdstew

    Gary Stewart wrote:

     

    "We're still waiting for the RasPi B+ schematics.  The RasPi page only has a single-pager with interfaces:"

     

    I have no idea why they have suddenly gotten secretive about this and it does not sit well with me that they have. Plus my attempts to get this changed have to date been ignored. I may wait until the schematics are(?) published before buying a Pi 2.

    My experience is that RasPi has always been slow about releasing schematics.  Speculating why is not particularly useful IMO -- it is what it is.  I don't think they've ever released Gerbers, which can be useful for understanding power distribution.

     

    RasPi is not open-source hardware.  This hasn't affected sales volume, so they have no incentive to change from proprietary.  For people who want OSHW, there are plenty of alternatives like BeagleBoard/Bone.  For people who just need schematics, there are even more alternatives.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Does anyone know if my B+ case works with Pi2?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago in reply to e14 Contributor

    Felix Chiu wrote:

     

    Does anyone know if my B+ case works with Pi2?

    Yes it does.  The external connectors are identical and in the same positions, according to this: http://www.element14.com/community/community/raspberry-pi/raspberrypi2

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to e14 Contributor

    Yes it has the same layout like John B says ...Should get mine this week, then I can confirm!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to johnbeetem

    Thanks! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to mcb1

    cpc.co.uk is where I ordered mine from, its an Element14 sister company if I remember correctly, got mine this morning so they are about, perhaps out of stock? Did order mine very quickly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 11 years ago in reply to johnbeetem

    "My experience is that RasPi has always been slow about releasing schematics."

     

    I said nothing about slow, I said secretive. It only took about two weeks to release the original schematics.

    Slow maybe, but not unreasonably so. The semi-useful B+ single page was released in about the same time

    frame, maybe a little longer. I haven't tried to download schematics for the model A, so I have no idea about

    them and I don't own an A+. It did take too long to get the BCM2835 specification published and even though

    it took much longer to get the GPU specification released, they are the first and only boards with an ARM SoC

    that has done so.

     

     

    "Speculating why is not particularly useful IMO -- it is what it is."

     

    No speculation about it in my post, I don't really care. As I said, I just want them to publish the full schematics

    of the B+ (all the Pi boards actually). I don't care if, for whatever reason, it takes them a month or two to do it.

    JUST DO IT.

     

     

    "RasPi is not open-source hardware"

     

    There is no ARM SoC open-source hardware, yet. Other than the Raspberry Pi, all ARM SoCs including the

    BeagleBone/Black use proprietary GPUs. Argue all you want, and you have before, you can't have open-

    source hardware with a large chunk of fully, undeniably, unarguably proprietary hardware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>