Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Microsoft and Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 682 subscribers
  • Views 2718 views
  • Users 0 members are here
  • microsoft
  • rasp-pi
  • raspberry_pi
  • development
  • windows_10
Related

Microsoft and Pi

markvenn
markvenn over 10 years ago

Today I got a mail from Microsoft Development Programme about the Pi and windows 10:

Hello Mark Venn,

 

We are super excited to announce a new addition to the IOT Developer Program – Raspberry Pi 2!

 

In partnership with the Raspberry Pi Foundation, we are going to make Windows 10 available for the Raspberry Pi 2. You’ll be among the first to know when we make Windows 10 available for the Raspberry Pi 2.

 

We will also continue to support the Intel Galileo through the program.

 

By being part of the Windows Developer Program for IoT you continue to be amongst the first to receive new information about the program, product announcements, beta program updates and launch specifics.

 

Thank you,
The Microsoft IoT Team

Microsoft Corporation
One Microsoft Way,
Redmond, WA, USA. 98052


I tried to get on the Galileo project to get a free board to play with, which is why I am on the list. I think quite a few people here on element14 are also on the program so we may get some early info as it appears.

I do not like the idea personally, we shall see how the treat the project. Am I alone in this?

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    Mark, you said,


    "I do not like the idea personally, we shall see how the treat the project. Am I alone in this?"


    I'm not quite sure what you don't like.


    I like the idea of Windows on RPi - and as I explained in another thread what would make it perfect would be a port of VB6 (or even QuickBasic) to Windows running on the Pi.

    That would make programming truly accessible to the zillions of people who can afford a Pi (it isn't just the money that holds people back).


    MK


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • markvenn
    markvenn over 10 years ago in reply to michaelkellett

    Michael

    What I do not like is the thought of MS possibly using this as leverage to get Linux off of the Pi and running windows exclusively. One of the benefits of the Pi is that it has not been, until now, in the MS camp and so offers a view of something different, letting people know that MS is not the only company making operating systems. There are enough machines running windows out there, some places should be left alone in my opinion. I suppose what I am saying is that I feel that this may be the thing end of the wedge.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 10 years ago in reply to markvenn

    I hope it is the thin end of the wedge:

     

    The Linux phenomenon has reached the point where it need a damn good kicking - I can run a 15 year old .exe file on windows 8 but I can't do the same with Linux - it comes in so many different and incompatible flavours that it's only useable by geeks.

     

    The great thing about early computers (Beebs, Spectrums, PCs) was that they were easy to get into and program. Windows made them easy to use but harder to program. Linux is hard to use and hard to program.

    For evidence of this look at the complexity of what you need to do use  a new peripheral (like the Wolfson/Cirrus) chip) with the Pi - can you just add a drive, no, you need to rebuild the kernel.

     

    Choice is good -  no one will be obliged to run Windows (I hope image)

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • royleith
    royleith over 10 years ago in reply to michaelkellett

    There are lots of old programs that I can run well on Linux (any distribution including Raspbian). There is lots of old hardware that I own that only runs on Linux since support has long since gone from Windows 7 and earlier. The support for the Wolfson/Cirrus card is still being developed. They will be able to use the new developments in Raspbian driver support to add the Cirrus driver to the main distribution. The Raspbian operating system is a special ARM development for the Pi. Nevertheless, I am running two of the older Wolfson cards and have written a mixer program for it using the tools already installed in the Raspi. While I wait for Cirrus, I just use the perfectly fine pre-compiled Raspbian distribution that they have provided.

     

    I have plugged and played DVD burners, USB serial ports, Flash drives, external hard drives, USB parallel ports and much more with Raspbian. Some of these are devices which no longer work in Windows because one cannot get up-to-date drivers. The Windows 10 OS for the Raspi will be the only one in use now that the Nokia Windows RT device and the Microsoft Surface RT have been binned. I doubt very much that there will be a huge army of companies and other developers building drivers and programs for the Raspi. Windows 10 is really a touchscreen based OS. We can only hope that they include generic drivers that support existing HDMI touchscreen monitors. However, as I see it, the point of a touchscreen on the Raspi is for something the size of a tablet. There are already such touchscreens with built-in support in Raspian. Microsoft will have to do the same at the same cost to make Windows 10 viable on the Raspi.

     

    Although Microsoft have released the free Visual Studio Lite for (Intel) desktops and laptops, I don't expect them to port any development tools to ARM for either the desktop environment or for apps on the tiled environment. Even if they did, it would be hard to get even a cut-down Windows 10 to run it with Raspi resources. Raspbian runs in 1.8GB. The Microsoft OS for the Intel equivalent board requires much more. From Microsoft's previous support for folk like us, I doubt we will ever get sufficient documentation and support to use it the way we use Raspbian. That's the issue with closed, proprietary operating systems.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Montala
    Montala over 10 years ago in reply to royleith

    Based on what has already been said, I think it is fair to say that it will indeed be a long time (if ever!) before we see Windows 10 included as an optional OS on NOOBS! image

     

    Mind you, by then we will probably be looking at the Raspberry Pi 3, complete with on-board wi-fi and Bluetooth support! image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Montala
    Montala over 10 years ago in reply to royleith

    Based on what has already been said, I think it is fair to say that it will indeed be a long time (if ever!) before we see Windows 10 included as an optional OS on NOOBS! image

     

    Mind you, by then we will probably be looking at the Raspberry Pi 3, complete with on-board wi-fi and Bluetooth support! image