Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Magnetic Door Switch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 709 subscribers
  • Views 2235 views
  • Users 0 members are here
  • raspberry_pi
Related

Magnetic Door Switch

e14 Contributor
e14 Contributor over 11 years ago

Hello,

 

I have a existing alarm system which has a magnetic door switch connected to it.  Would it be ok to connect the same switch to the PI?  i.e. connect a pair of wires  from the PI to the same input as the switch on the alarm panel?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks guys!

     

    The more I think about this, the more I'm going towards changing the alarm panel to one which  I can fully integrate with the PI.  Ideally using something like this AD2USB, The AlarmDecoder Store which taps in to the alarm panel ports used to monitor the alarm.  The only issue is that I can't find an alarm panel which is compatible with this device and available in the uk.

     

    My goal is made of 2 parts, one is to use the existing PIRs and reed switches to use as inputs in the PI so I can control the lights in the house.  Secondly I'd like to monitor my alarm system and be able to change the state of the alarm remotely. ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    Hi shyambhundia

     

    Looks like an interesting module you've found there. I would investigate USB driver compatibility with the Pi before purchasing. You could also look into the RS232 version they produce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Yep, thats on my checklist..But i've seen it being done on another blog..ill see if i can dig it out.  They also do a PI version too.

     

    But I need to find a panel first image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Yep, thats on my checklist..But i've seen it being done on another blog..ill see if i can dig it out.  They also do a PI version too.

     

    But I need to find a panel first image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor

    Good luck finding one. image