Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 "5 V Power Supply" Notes
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 680 subscribers
  • Views 3633 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi 2 "5 V Power Supply" Notes

Former Member
Former Member over 10 years ago

Some time ago, I ordered and received the RPi 2,.  ordered and imaged a new SD card and found the board not booting.

 

Having been using a RPi 1 with power supply, monitor, mouse and keyboard and never seen any problems starting,. I expected

the new board also to boot with the new SD card and the rest of the hardware.

 

After spending quite some time with changing to another RPi 2 board ( exchange )  different SD cards, I had the conclude that

my problem most likely had to do with the the power supply.

 

All the used SD cards and hardware  did work with The RPi 1.

 

Up to this point both boards did not work while the RP1 1 never failed to boot.

 

The power supply I was using provided about 5.4 V measured on the miniature USB connector on the board. Changing start sequence

had no effect, 110 Volt first, USB switching with Power Supply already powered up. No variations in the board voltage were noticed.

during the start-up.

 

The power supply ( Chinese switching ) had a relative thin output power cord ( by closer inspection )

 

Finally, by using an home built power supply with adjustable output voltage and the heavier gauge output power cord, I got both computer

board to work with all the SD cards I had required in the previous process.

 

Not having an oscilloscope available, I was not able to look for any non wanted effects at the time of switching on the RPi 2.

My final conclusion is that the RP1 2 is much more sensitive to possible voltage changes than the RPi 1 during start-up and booting

With the adjustable 5 V power, I experienced no problems running between 4.5 and 5.5 V input to the board.

 

Wished I had known this a little earlier....!

 

Rein Smit

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Certainly when I was learning Electronics with the good old TTL and CMOS chips along with the CPU/ ROM/ GPIO chips of the time, it was all 5V +/- 5%, not 10% but having looked at a few of the common PDF details for some chips I'm using now, they are indeed all 10% (1970s - 1990s) compared to 2015

     

    This does not imply ALL chips are now 10%, just that some are, so I would still be cautious of assuming 10% is good for all and as has already been stated, without schematics no-one can be sure

     

    On a separate note, this is a USB connector and the PSU can be (And at some point will be) used on other devices. the USB specification clearly states +5%, - 11% so between 4.45 and 5.25V MAX. but up to 5A in the case of a charging interface so a wall brick with USB interface outputting more than 5.25V is OUT OF SPECIFICATION.

     

    Hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes

    The issue with most of these chargers ... are just that.

    They are designed to charge the battery of the device they were supplied for.

     

    A 3.7/4.1v battery doesn't really care what voltage it gets so long as it is enough for the charging circuit.

     

    Sadly some of the recommended power packs supplied are not up to the job.

     

    I haven't tried to find a 2A version, so I can't say which one will work.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to mcb1

    Similarly, most of the 'pi is designed to run off a 3.7V lithium battery. So also the 'pi doesn't care what voltage it gets.

     

    This argument breaks down for:
    * HDMI: The pi should provide some 5V power on the connector. The HDMI->VGA converters rely on this.

    * USB: The pi should provide 5V to the USB devices. If this voltage is outside spec, some USB devices refuse to work.

     

    The first 'pi had a "lowsy" 3.3V regulator. It required a voltage drop of at least 1V to operate. This means a 5V on the pi of 4.3V was required to keep the 3.3V on the pi in regulation. I expect that a new pi2 has a much lower dropout on the 3.3V and will operate just fine at 3.4V on its 5V line.... (But I haven't tried it yet, so I might be wrong).

     

    Let me back up my claims and I'll report back today with measurements, ok?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 10 years ago in reply to mcb1

    Similarly, most of the 'pi is designed to run off a 3.7V lithium battery. So also the 'pi doesn't care what voltage it gets.

     

    This argument breaks down for:
    * HDMI: The pi should provide some 5V power on the connector. The HDMI->VGA converters rely on this.

    * USB: The pi should provide 5V to the USB devices. If this voltage is outside spec, some USB devices refuse to work.

     

    The first 'pi had a "lowsy" 3.3V regulator. It required a voltage drop of at least 1V to operate. This means a 5V on the pi of 4.3V was required to keep the 3.3V on the pi in regulation. I expect that a new pi2 has a much lower dropout on the 3.3V and will operate just fine at 3.4V on its 5V line.... (But I haven't tried it yet, so I might be wrong).

     

    Let me back up my claims and I'll report back today with measurements, ok?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to rew

    Afraid to say that you are, the PI2 even has built in voltage monitor and it triggers around 4.65ish volts, this is indicated by the small rainbow square showing up in the top right corner of the console and indicates a low input voltage is detected.

     

    On several of my PI2's I have observed issues even with standard USB adapters but poorer USB leads triggering this indicator and in some cases the PI2 even will hang. The PI2 may well have better regulators (Buck vs Linear) but it is actually worse for tollerating lower input voltages

     

    I will do a video on this soon showing a formal test of input volts over stability , jsut need to get a few other things out of the way first

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to Robert Peter Oakes

    Peter you are right about the newer Raspberry Pi are voltage tolerant as long as 5 volts +/- 10%. Otherwise the artefact will occur in upper right corner warning about low voltage. I first saw this on my Pi 2.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago in reply to clem57

    OK.

    I ran the tests......

     

    When slowly decreasing voltage, I seem to be able to reach voltages BELOW 3.3V, and keep the 'pi running.

    When booting, a voltage of about 3.5V seems to be required.

     

    I've spent a good part of the last two weeks debugging power-problems on one of my own designs. So I've gathered a bit of experience. I'm guessing that during boot a short power-spike causes things to drop even further. My previous measurements on the first 'pi indicated that the LAN chip is the critical part. It requires 3.3V +/- 10%, and will continue to work (as specified) down to about 3.0V. As predicted the dropout of the switching regulator for the 3.3V is a lot less than the dropout of the 1117 on the first pi. And about 0.2V sounds about right for the dropout of such a regulator. Current spikes while booting probably cause a drop below 3.0V.

     

    My pi currently runs at 0.25A at 5V (1.25W), while it booted at 3.5V and ended up with 0.35A (1.22W). So the difference in power consumption is very small.

     

    Note that I've taken care to remove all possible 5V-requiring peripherals.

     

    Also note that by lowering the voltage below 3.3V I've risked damaging my SD card. The SD card also runs from 3.3V.

     

    One funny thing: My power led has not come back on now that the voltage is back at 5.0V after booting at 3.5V.....

     

    So..... For battery applications, you are better off running the pi directly from a lithium ion battery than transforming the battery voltage to 5.0V (probably at 80% efficiency). Then, if you have 5V peripherals, you should arrange to feed them separately: you're saving about 0.2W by not passing the power for the pi itself through the step up converter.

     

    [update: The pi boots just fine with only 3.2V, I was using bad leads to power it.....]

    [update2: Still boots with 2.93V (doesn't boot with 2.7V, even though it remains running at that voltage)..... ]