Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problem of booting raspberry Pi model B
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 696 subscribers
  • Views 2630 views
  • Users 0 members are here
  • raspberry_pi
Related

Problem of booting raspberry Pi model B

Former Member
Former Member over 10 years ago

I get the error message,

sh: can't access tty: job control turned off
/ #.

I have try to format my SD card, remove all the USB devices. The message is still there even though there is only my SD card and screen adapter.

I appreciate if any expert help me.I am doing my FYP now, need answer asap.thx

  • Sign in to reply
  • Cancel
  • clem57
    clem57 over 10 years ago

    If you have hardware attached your GPIO pins, try removing them. It maybe a hardware error

    Otherwise add avoid_safe_mode=1 to config.txt in /boot

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    I would sugest a fresh install of the OS including download from the Raspberry PI website. You have not mentioned what you have tried so far of what OS your working with so Im assuming Raspbian

     

    I have installed numerous PIs and everyone without fail has worked with no requirement to start adding things to config.txt or anyother file for that matter to enable remote SSH.

     

    with only HDMI screen, keyboard and mouse, I simply setup the menu when prompted enduring SSH is enabled (Though I beleve SSH is enable by default ?)

     

    Basic things to check

    Power supply is providing 5V at the PI, requires a good USB cable

    Supported keyboard and Mouse

    HDMI screen preferably

     

    What types of equipment do you have hooked up to the PI ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 10 years ago

    This message means that your shell is running on the CONSOLE (/dev/console), not on /dev/tty1 or something like that.

     

    It happens if you boot your Linux system with "init=/bin/sh" or tricks like that.

     

    (the console is available from really early in the booting-the-kernel process. It does not have things like... job control, the actual tty-console  gets initialized a bit later, and uses the same hardware.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to clem57

    the boot file is in the OS, Respian?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    Yeah, I am using Raspbian. But, I think there is no OS in my Raspbian as my screen just popped out the message in the halfway of Raspbian installation.

    So far, even though there is no equipment except my screen, my PI wont work also image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to rew

    I dont get what ur meaning. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member

    You should try using an SD card that is a CLASS 10 and as fast as you can, I would say 40MBytes/Sec or better, use the proper SD card formatter and install Noobs onto the card as described on my video or the Raspberry PI web site

     

    is it a PI 2 or an earlier model ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Robert Peter Oakes

    Thank you for you all guys help. I can boot my PI by writing Raspbian image to my SD card using the Win32DiskImager.

    • Cancel
    • Vote Up +1 Vote Down