Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29215 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Matthias!

     

    I am just a Linux tinkerer and know only enough to be dangerous. I have a live nature audio streaming website that I have been using Raspi B+ with Darkice for streaming. I wanted to upgrade to Pi 3 with Cirrus Logic audio running Darkice. I have tried numerous times to upgrade the Raspi B+ image to Pi 3 with the Cirrus logic card support and have the same result. Once I reach the point of having my Darkice image upgrade to Pi 3 I check aplay -l I get the message that the Raspi internal audio adapter is there. After I include your recommended updates of installing the 4.4.14 pre-compile kernel, make the additions to /boot/config.txt, generate the /etc/modprobe.d/cirrus.conf file with the required content, then reboot, I running the aplay -l command. A message is displayed that I have no audio adapters available.

     

    I have added dtdebug=1 to the /boot/config.txt, rebooted the system then tried to use the paste command as you describe in your instructions to collect the information needed for debug. After reading through many of the postings on thread, I saw where you talked about the paste command providing a url that would referenced the location of the data I have collected. When I used the paste command, it acts like a cat command and displays results on the terminal that I am entering the command into. I can't figure out where that url is located. I did copy the output displayed in the terminal and have it available in a file that's about 80KB in size.

     

    I believe that you would take one look at this information and see what I am doing wrong. I know that what I am trying to do is possible because I read where other people before have made the Raspi 3, Cirrus Logic, Darkice combination work.

     

    Could you suggest some way that I could get this file with the results of the paste command to you? Once I figure out how the get this combination of hardware/software to work, I would like to make the image available to future Linux novices that would like to have it. I know Grant from Soundtent has expressed interest in a copy of the image.

     

    Additionally, once I get past the issue with the audio adapter being operational, I will have a question about; Note: You have to start the appropriate scripts before you can use the card. For example:. Can I just put the play command, ./Playback_to_Lineout.sh -q, in rc.local so the Cirrus audio card will be ready to stream once the Raspi has completed the boot process?

     

    Thanks for both making the functioning combination of Pi 3 and the Sirrus Logic audio card doable and for all the time you put into helping novice Linux users, like myself, make this stuff work! Sorry about all these words just to ask two questions.

     

    BTW - If you are curious about the website: livenaturesongs,com.

     

    Sincerely,

     

    Joel Goodwin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Matthias!

     

    I am just a Linux tinkerer and know only enough to be dangerous. I have a live nature audio streaming website that I have been using Raspi B+ with Darkice for streaming. I wanted to upgrade to Pi 3 with Cirrus Logic audio running Darkice. I have tried numerous times to upgrade the Raspi B+ image to Pi 3 with the Cirrus logic card support and have the same result. Once I reach the point of having my Darkice image upgrade to Pi 3 I check aplay -l I get the message that the Raspi internal audio adapter is there. After I include your recommended updates of installing the 4.4.14 pre-compile kernel, make the additions to /boot/config.txt, generate the /etc/modprobe.d/cirrus.conf file with the required content, then reboot, I running the aplay -l command. A message is displayed that I have no audio adapters available.

     

    I have added dtdebug=1 to the /boot/config.txt, rebooted the system then tried to use the paste command as you describe in your instructions to collect the information needed for debug. After reading through many of the postings on thread, I saw where you talked about the paste command providing a url that would referenced the location of the data I have collected. When I used the paste command, it acts like a cat command and displays results on the terminal that I am entering the command into. I can't figure out where that url is located. I did copy the output displayed in the terminal and have it available in a file that's about 80KB in size.

     

    I believe that you would take one look at this information and see what I am doing wrong. I know that what I am trying to do is possible because I read where other people before have made the Raspi 3, Cirrus Logic, Darkice combination work.

     

    Could you suggest some way that I could get this file with the results of the paste command to you? Once I figure out how the get this combination of hardware/software to work, I would like to make the image available to future Linux novices that would like to have it. I know Grant from Soundtent has expressed interest in a copy of the image.

     

    Additionally, once I get past the issue with the audio adapter being operational, I will have a question about; Note: You have to start the appropriate scripts before you can use the card. For example:. Can I just put the play command, ./Playback_to_Lineout.sh -q, in rc.local so the Cirrus audio card will be ready to stream once the Raspi has completed the boot process?

     

    Thanks for both making the functioning combination of Pi 3 and the Sirrus Logic audio card doable and for all the time you put into helping novice Linux users, like myself, make this stuff work! Sorry about all these words just to ask two questions.

     

    BTW - If you are curious about the website: livenaturesongs,com.

     

    Sincerely,

     

    Joel Goodwin