Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29004 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • hiassoft
    hiassoft over 10 years ago

    If you don't want to compile yourself, here's a precompiled 4.1.6+ kernel (tested with original Wolfson card on RPi B and Cirrus card on RPi 2):

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.1.6.tgz

     

    As already mentioned you need to add 2 softdep lines to your modprobe configuration. Here's my /etc/modprobe.d/cirrus.conf file:

     

    softdep arizona-spi pre: arizona-ldo1
    softdep spi-bcm2708 pre: fixed
    softdep spi-bcm2835 pre: fixed
    softdep snd-soc-wm8804-i2c pre: snd-soc-rpi-wsp-preinit
    softdep snd-soc-rpi-wsp pre: snd-soc-wm8804-i2c

     

    Some background info about this new change:

     

    The Wolfson/Cirrus driver (snd-soc-rpi-wsp/rpi-cirrus-sound-pi.c) contained code to reset the wm8804 chip and initialize it to I2C mode by directly switching the GPIO pins, including the I2C pins. Unfortunately, this interfers with the Linux (deferred) driver loading mechanism. This WM8804 init code was called on each try to init the Cirrus driver which led to quite long delays until the driver would be loaded and, even worse, it could interfere with the WM8804 I2C detection. If WM8804 I2C detection is run when the Cirrus driver has taken over the GPIO pins the detection will fail and you end up with a non-working card.

     

    I ended up with the current solution, moving this one-time init code into a separate module and adding softdeps to ensure this WM8804 init is done before WM8804 detection and Cirrus driver loading. It's kind of a hack and I'm not 100% happy with the solution, but it seems to work fine. If someone has a better idea how to solve this, I'd be glad to hear about it!

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Matthias,

     

    Hi, I apologize for being lame, but can you post an SD card full raspbian image to google drive or dropbox or an ftp download site so I can just try your solution.  I am out of ammo and time on building kernels and can't even get a 3.18.16 image, it is a 3.18.10 on the web site.  I have huge SD cards so if the image is large that is not a problem and I can reduce it for re-sharing.  I am sure that lots of folks will be interested in a decent, modern, driver leak fixed Wolfson Audio/Pi B and Pi 2 Raspbian image.  I'd be happy to host the image on our web site.  Really Cirrus Logic ought to host a correct, bug free image.

     

    Thanks for your hard work and consideration,

     

    Shannon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Hi Shannon!

     

    Sorry, I can't provide an image. One reason is that my DSL upload speed really sucks, the other reason is that I'm not a huge fan of prebuilt images.

     

    Instead just do the following:

    • Do a standard raspbian installation, configure it to your likes (eg get rid of all that desktop stuff if you don't need it)
    • Do a "sudo apt-mark hold raspberrypi-bootloader" so that further raspbian updates won't overwrite the custom Cirrus kernel
    • Download the precompiled Cirrus kernel from this thread and the usecase scripts and install them (unpack the kernel in the root directory, as user root, unpack the usescase script tarball somewhere you like - eg /usr/local/bin or /home/pi/bin)
    • Edit /boot/config.txt and create the /etc/modprobe.d/cirrus.conf file as described

     

    That's all you need to do.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Hi Shannon!

     

    Sorry, I can't provide an image. One reason is that my DSL upload speed really sucks, the other reason is that I'm not a huge fan of prebuilt images.

     

    Instead just do the following:

    • Do a standard raspbian installation, configure it to your likes (eg get rid of all that desktop stuff if you don't need it)
    • Do a "sudo apt-mark hold raspberrypi-bootloader" so that further raspbian updates won't overwrite the custom Cirrus kernel
    • Download the precompiled Cirrus kernel from this thread and the usecase scripts and install them (unpack the kernel in the root directory, as user root, unpack the usescase script tarball somewhere you like - eg /usr/local/bin or /home/pi/bin)
    • Edit /boot/config.txt and create the /etc/modprobe.d/cirrus.conf file as described

     

    That's all you need to do.

     

    so long,

     

    Hias