Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 28898 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • markzed
    markzed over 11 years ago

    Thanks a bunch for doing this. For those of us who are really noobs (like me) here are detailed instructions.

     

    For 3.18.16

     

    • Get the 3.18.16 raspbian image. I used the Raspbian image provided by Raspberry Pi org here: https://www.raspberrypi.org/downloads/
    • Do what you need to create the SD image, test it, expand it - see the Raspbian doc for this
    • Once you've verified it's working, untar the image pointed to in the main post:

    cd /

    sudo tar -xvzf path-to-the-gz-file

    sudo nano /boot/config.txt

      • add these two lines to the end of the config.txt file

    dtoverlay=rpi-cirrus-wm5102-overlay

    dtoverlay=i2s-mmap

    sudo nano /etc/modprobe.d/raspi-blacklist.conf

      • note the file may not be already there
      • add the three lines shown in the first post to the end of the file

    softdep arizona-spi pre: arizona-ldo1 

    softdep spi-bcm2708 pre: fixed 

    softdep spi-bcm2835 pre: fixed 

     

    Now reboot, via     sudo reboot


    To verify that everything is ok, type     aplay -l      in a terminal window and the first card should be sndrpiwsp shown as a WM5102

     

    Next, you'll want the scripts from Wolfson that make things straightforward. To get those, in a terminal window type (this is from https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code)

     

    cd ~
    git clone --depth 1 https://github.com/CirrusLogic/wiki-content.git
    mv wiki-content/scripts/* ~/
    chmod +x *.sh

     

    To really test this you can use aplay but it has limited support. I installed mplayer and had to edit my ~/.asoundrc file to point to card 0 by default. This plays well:

     

    mplayer -srate 96000 -format s32le music-file-path

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • markzed
    markzed over 11 years ago

    Thanks a bunch for doing this. For those of us who are really noobs (like me) here are detailed instructions.

     

    For 3.18.16

     

    • Get the 3.18.16 raspbian image. I used the Raspbian image provided by Raspberry Pi org here: https://www.raspberrypi.org/downloads/
    • Do what you need to create the SD image, test it, expand it - see the Raspbian doc for this
    • Once you've verified it's working, untar the image pointed to in the main post:

    cd /

    sudo tar -xvzf path-to-the-gz-file

    sudo nano /boot/config.txt

      • add these two lines to the end of the config.txt file

    dtoverlay=rpi-cirrus-wm5102-overlay

    dtoverlay=i2s-mmap

    sudo nano /etc/modprobe.d/raspi-blacklist.conf

      • note the file may not be already there
      • add the three lines shown in the first post to the end of the file

    softdep arizona-spi pre: arizona-ldo1 

    softdep spi-bcm2708 pre: fixed 

    softdep spi-bcm2835 pre: fixed 

     

    Now reboot, via     sudo reboot


    To verify that everything is ok, type     aplay -l      in a terminal window and the first card should be sndrpiwsp shown as a WM5102

     

    Next, you'll want the scripts from Wolfson that make things straightforward. To get those, in a terminal window type (this is from https://github.com/CirrusLogic/rpi-linux/wiki/Building-the-code)

     

    cd ~
    git clone --depth 1 https://github.com/CirrusLogic/wiki-content.git
    mv wiki-content/scripts/* ~/
    chmod +x *.sh

     

    To really test this you can use aplay but it has limited support. I installed mplayer and had to edit my ~/.asoundrc file to point to card 0 by default. This plays well:

     

    mplayer -srate 96000 -format s32le music-file-path