Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29112 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • hiassoft
    hiassoft over 10 years ago

    I've uploaded an updated version, based on the freshly released 4.1.16 kernel:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.1.16.tgz

     

    As usual the source is on github: https://github.com/HiassofT/rpi-linux/tree/cirrus-4.1.16

     

    I've reworked some of my previous fixes, especially the one which tried to fix switching between 44.1kHz-related and 48kHz-related rates (which resulted in wrong playback rate with the original driver).

     

    The original quick-fix, bringing back the FLL setup into snd_rpi_wsp_config_5102_clks, caused several issues: Whenever one started a recording when playback was running (or vice versa) we got short dropouts/clicks. And, what's even worse, on rare occasions this fix could "confuse" the chip and we ended up with an even more off sample rate.

     

    I've now implemented a (hopefully) proper fix for this and also back-ported some wm5102/arizona related fixes from newer kernel versions.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hiassoft
    hiassoft over 10 years ago

    I've uploaded an updated version, based on the freshly released 4.1.16 kernel:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.1.16.tgz

     

    As usual the source is on github: https://github.com/HiassofT/rpi-linux/tree/cirrus-4.1.16

     

    I've reworked some of my previous fixes, especially the one which tried to fix switching between 44.1kHz-related and 48kHz-related rates (which resulted in wrong playback rate with the original driver).

     

    The original quick-fix, bringing back the FLL setup into snd_rpi_wsp_config_5102_clks, caused several issues: Whenever one started a recording when playback was running (or vice versa) we got short dropouts/clicks. And, what's even worse, on rare occasions this fix could "confuse" the chip and we ended up with an even more off sample rate.

     

    I've now implemented a (hopefully) proper fix for this and also back-ported some wm5102/arizona related fixes from newer kernel versions.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Many thanks for updated kernel source.

     

    I've updated PKGBUILD at GitHub.

    Additionally there are ready to install kernel packages. You can find them at headless.audio.

     

    Ed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Thanks for your great work!

    I downloaded the 4.1.16 source code and compile sucefully on rpi1,

    and i sucefully hear the music from mpd.

    but there are some error message from dmesg.

    system:raspbian-jessie-lite 2016-02-06

    pi@Wolfson:~ $ aplay -l

    **** List of PLAYBACK Hardware Devices ****

    card 0: sndrpiwsp [snd_rpi_wsp], device 0: WM5102 AiFi wm5102-aif1-0 []

      Subdevices: 0/1

      Subdevice #0: subdevice #0

    pi@Wolfson:~ $ dmesg | grep snd-rpi

    [    9.980438] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [    9.980453] snd-rpi-wsp sound: Failed to register card: -517

    [   10.756252] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [   10.756281] snd-rpi-wsp sound: Failed to register card: -517

    [   12.941450] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [   12.941491] snd-rpi-wsp sound: Failed to register card: -517

    [   12.959889] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [   12.959924] snd-rpi-wsp sound: Failed to register card: -517

    [   12.987564] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [   12.987596] snd-rpi-wsp sound: Failed to register card: -517

    [   12.988953] snd-rpi-wsp sound: ASoC: CPU DAI (null) not registered

    [   12.988987] snd-rpi-wsp sound: Failed to register card: -517

    [   12.991259] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   12.991290] snd-rpi-wsp sound: Failed to register card: -517

    [   12.992325] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   12.992360] snd-rpi-wsp sound: Failed to register card: -517

    [   13.071121] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   13.071153] snd-rpi-wsp sound: Failed to register card: -517

    [   13.290994] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   13.291034] snd-rpi-wsp sound: Failed to register card: -517

    [   13.370104] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   13.370144] snd-rpi-wsp sound: Failed to register card: -517

    [   13.490198] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   13.490242] snd-rpi-wsp sound: Failed to register card: -517

    [   13.504786] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    [   13.504825] snd-rpi-wsp sound: Failed to register card: -517

    [   16.589497] snd-rpi-wsp sound: wm5102-aif1 <-> 20203000.i2s mapping ok

     

    cat /boot/config.txt

    dtoverlay=rpi-cirrus-wm5102

    dtoverlay=i2s-mmap

    dtdebug=1

     

    pi@Wolfson:~ $ vcdbg

    debug_sym: OpenVideoCoreMemoryFileWithOffset: Unable to open '/dev/vc-mem': Permission denied(13)

     

    pi@Wolfson:~ $ cat /etc/modprobe.d/cirrus.conf

    softdep arizona-spi pre: arizona-ldo1

    softdep spi-bcm2708 pre: fixed

    softdep spi-bcm2835 pre: fixed

    softdep snd-soc-wm8804-i2c pre: snd-soc-rpi-wsp-preinit

    softdep snd-soc-rpi-wsp pre: snd-soc-wm8804-i2c

     

    Unable to open videocore memory access: -13

     

    share my mpd settings.

    /etc/mpd.conf

    audio_output {

            type            "alsa"

            name            "My ALSA Device"

            device          "hw:0,0"        # optional

            mixer_device    "hw:0"  # optional

            mixer_control   "HPOUT1 Digital"                # optional

            mixer_index     "0"             # optional

    }

     

    It alwanys prompt  Failed to register card: -517,but the wolfson audio card did work.why there are so many error prompt?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    李 逍遥 schrieb:

     

    It alwanys prompt  Failed to register card: -517,but the wolfson audio card did work.why there are so many error prompt?

    -517 is -EPROBE_DEFER, that is the kernel deferred probing mechanism. It's not an actual error, just means some of the other components weren't available (in your case the bcm2708 I2S driver and the wm5102 driver) and that the kernel should retry later.

     

    Long story short: just ignore these messages if you finally get the "mapping ok" message.

     

    so long,

     

    Hias