Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29090 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • hiassoft
    hiassoft over 10 years ago

    I just uploaded a new kernel, based on 4.1.18:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.1.18.tgz

     

    No changes in the audio driver, but some USB and MMC fixes in the RPi tree.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hias,

     

    the version 4.1.18 contains the comment:

    cirrus: silence probe deferral messages from register card

    The reason for the probe deferral (eg DAI not registered) is already

    logged, so there's no need for further dmesg spam

    So indeed the message

    snd-rpi-wsp sound: Failed to register card: -517

    has gone.

     

    But still there is the dmesg spam like

     

    [5.245000] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.249957] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.361766] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.372619] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.513485] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.582022] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.609680] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.610961] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [6.069378] snd-rpi-wsp sound: wm5102-aif1 <-> 3f203000.i2s mapping ok

     

    So it may make sense to also remove it.

     

    Uli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hias,

     

    the version 4.1.18 contains the comment:

    cirrus: silence probe deferral messages from register card

    The reason for the probe deferral (eg DAI not registered) is already

    logged, so there's no need for further dmesg spam

    So indeed the message

    snd-rpi-wsp sound: Failed to register card: -517

    has gone.

     

    But still there is the dmesg spam like

     

    [5.245000] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.249957] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.361766] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.372619] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.513485] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.582022] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.609680] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [5.610961] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered
    [6.069378] snd-rpi-wsp sound: wm5102-aif1 <-> 3f203000.i2s mapping ok

     

    So it may make sense to also remove it.

     

    Uli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Hi Uli!

     

    But still there is the dmesg spam like

     

    [5.245000] snd-rpi-wsp sound: ASoC: CODEC DAI wm5102-aif1 not registered

    These messages are coming from the ASoC layer and I didn't want to touch these. I only silenced the messages from the Cirrus driver because they are somewhat redundant (ASoC already logged which device was missing) and they seemed to scare users - I received a lot of questions what this error -517 was.

     

    There have been several discussions on the kernel mailing lists how to deal with the probe deferral messages. Ideally you'd just get a single error message with all the details when the deferred probing mechanism finally failed. But this is rather tricky to do and so far there's no real solution to that yet. Obviously we can't silence all deferred probing messages, otherwise there'd be no easy way to find out what exactly went wrong in case of a real error.

     

    Until there's some accepted solution in upstream we just have to live with these (few) repeated log messages.

     

    so long,

     

    Hias