Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29090 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • hiassoft
    hiassoft over 10 years ago

    I've uploaded a new kernel build, based upon 4.1.19:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.1.19.tgz

     

    I finally found out what was causing the issues on the new RPi3 (other soundcards where effected as well), this kernel build contains all the needed patches. Note: be sure you have a very recent Raspbian installation or update the GPU firmware if you are using a RPi3.

     

    Other changes in this build:

    • Add missing .owner field in snd_soc_card
      This prevents module unloading while the card is in use (which leads to a kernel crash) and makes ALSA slot ordering working.
    • Silence probe deferral messages from register card

     

    I've updated the docs on my webpage and added instructions how to use the slot ordering and how to disable the RPi on-board audio device

    http://www.horus.com/~hias/cirrus-driver.html

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hi,

     

    Today I acquired a Cirrus Audio Card and tested it with the kernel build 4.1.19. Everything works great until I load the experimental OpenGL support by adding dtoverlay=vc4-kms-v3d to /boot/config.txt -- The Cirrus card is nowhere to be found.

     

    Combing through dmesg I found this:

    bcm2708-i2s 3f203000.i2s: can't request region for resource [mem 0x3f101098-0x3f10109f]

    bcm2708-i2s: probe of 3f203000.i2s failed with error -16

     

    vc4-kms-v3d-overlay.dts doesn't seem to mention anything about using i2s so I'm stumped on what's the issue.

     

    Any hope or hints for further debugging?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hi,

     

    Today I acquired a Cirrus Audio Card and tested it with the kernel build 4.1.19. Everything works great until I load the experimental OpenGL support by adding dtoverlay=vc4-kms-v3d to /boot/config.txt -- The Cirrus card is nowhere to be found.

     

    Combing through dmesg I found this:

    bcm2708-i2s 3f203000.i2s: can't request region for resource [mem 0x3f101098-0x3f10109f]

    bcm2708-i2s: probe of 3f203000.i2s failed with error -16

     

    vc4-kms-v3d-overlay.dts doesn't seem to mention anything about using i2s so I'm stumped on what's the issue.

     

    Any hope or hints for further debugging?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    This overlays the device tree not adds to it. Check it out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Currently I2S soundcards and the VC4 drm driver can't be used at the same time.

     

    The vc4 driver uses the clock framework (which manages all clocks of the SoC) but the I2S driver hasn't yet been converted to use the clock framework. So what's happening here is that the clock framework grabs the memory locations of all the clocks, bcm2708-i2s tries to grab the locations of the PCM clock as well, but fails because they are already used by the clock framework.

     

    There's already been some work to convert the bcm I2S driver to use the clock framework, but it's not that simple and it hasn't been included in the upstream kerrnel yet. Read this (rather lengthy) discussion on github for details:

    https://github.com/raspberrypi/linux/issues/1231

     

    so long,

     

    Hias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Thanks for the quick and accurate answer. So there's hope that some day it will work...