Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29112 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello,

     

    I recently purchased a Raspberry Pi 3 and Cirrus Logic Audio Card and have followed the instructions on this page to install the Audio Card using Noobs 1.9.0.

    I can see the card show up in "Audio Device Settings" as "snd_rpi_wsp (Alsa mixer) (Default)". But, when I try to choose the card in any audio program such as Sunvox or Jack - i.e. "hw:sndrpiwsp" or (hw:0,0) the card does not work. Instead, for instance, Sunvox will not load and hangs using Alsa and/or Jack gives me error "Could not connect to JACK server as client.

     

    I notice that when I power on my RPI 3 with Cirrus Logic card I see Red and Green lights on the Cirrus card then it switches to just Green when booting Noobs.

     

    My goal here is to connect and use the SPDIF in and outs of the Cirrus card to a Pro Tools Avid HD Omni system. I want to use SunVox as an external synthesizer to Pro Tools.

     

    I am new to the RPI world and the last time I use Linux was almost 20 years ago but this was very easy to setup and follow the instructions on

      RPi Linux driver for Wolfson / Cirrus Logic Audio Card

     

    Any help would be very appreciated

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello,

     

    I recently purchased a Raspberry Pi 3 and Cirrus Logic Audio Card and have followed the instructions on this page to install the Audio Card using Noobs 1.9.0.

    I can see the card show up in "Audio Device Settings" as "snd_rpi_wsp (Alsa mixer) (Default)". But, when I try to choose the card in any audio program such as Sunvox or Jack - i.e. "hw:sndrpiwsp" or (hw:0,0) the card does not work. Instead, for instance, Sunvox will not load and hangs using Alsa and/or Jack gives me error "Could not connect to JACK server as client.

     

    I notice that when I power on my RPI 3 with Cirrus Logic card I see Red and Green lights on the Cirrus card then it switches to just Green when booting Noobs.

     

    My goal here is to connect and use the SPDIF in and outs of the Cirrus card to a Pro Tools Avid HD Omni system. I want to use SunVox as an external synthesizer to Pro Tools.

     

    I am new to the RPI world and the last time I use Linux was almost 20 years ago but this was very easy to setup and follow the instructions on

      RPi Linux driver for Wolfson / Cirrus Logic Audio Card

     

    Any help would be very appreciated

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hiassoft
    hiassoft over 10 years ago in reply to e14 Contributor

    Hi Alex!

    I can see the card show up in "Audio Device Settings" as "snd_rpi_wsp (Alsa mixer) (Default)". But, when I try to choose the card in any audio program such as Sunvox or Jack - i.e. "hw:sndrpiwsp" or (hw:0,0) the card does not work. Instead, for instance, Sunvox will not load and hangs using Alsa and/or Jack gives me error "Could not connect to JACK server as client.

    You probably just forgot to run the "usecase" scripts. I've updated that section on my website, for SPDIF in/out you'll have to do this:

    ./Reset_paths.sh -q
    ./SPDIF_playback.sh -q
    ./SPDIF_record.sh -q

     

    Enabling the other playback paths (lineout, headset) as well won't hurt, the can be active in parallel.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to hiassoft

    Hi,

     

    Thanks for responding so quickly Hias.

     

    You are correct. I did not install "usecase" scripts.

     

    Everything works now!

     

    Thank you for adding the new instructions on your site. I followed them exactly.

     

    All the best,

     

    Alex