Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29112 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • binauralhead
    binauralhead over 10 years ago

    Hi there, tried downloading some of the images, however, on extraction there are quite a few files that are already written, and asks if I want to overwrite them, some have different kb sizes, not sure what is going on there, any pointers?

     

    I have just received my first raspi3 with the cirrus logic card, works great on the piB with other images, but those "other" images do not work on the raspi3.

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiassoft
    hiassoft over 10 years ago in reply to binauralhead

    Hi Alan!

     

    What exactly to you mean by "other" images? How did you extract the files, when did you get the "overwrite" messages?

     

    For the RPi3 you need the very latest kernel, currently 4.1.19. Also follow the instructions on my website:

    RPi Linux driver for Wolfson / Cirrus Logic Audio Card

     

    The precompiled kernel overwrites quite some files (kernel.img, dtb/overlay files, modules if you have kernel 4.1.19 already installed), but normally extracting with tar will silently overwrite them. Unless you forgot to extract as root or use sudo, then it can't overwrite these files and will complain loudly.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 10 years ago in reply to hiassoft

    Hello Hias,

     

    When I extract the file cirrus-linux-4.1.19.tgz (using windows PC) extract to a new folder, as the image is being extracted, the files being written from the folder "lib" - there are quite a few files (9) with the same name, but different files sizes, I get prompted to either overwrite or skip them. Not sure why there are already files written as they should all be unique. Quite confused about that!

     

    The first two are shown below.

     

    image

    image

     

    Anyway I was hoping they would be extracted so that I could then copy them to the Pi3's SD card.

     

    I'm a bit of a noob, but have several Pi's, but not had any experience with Pi2's or Pi3's though.

     

    I'm just playing with a NOOBS image that can boot the Pi3, and seeing if I can manage to get darkice to install.

     

    But any help in the mean time would be welcomed.

     

    Regards

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • binauralhead
    binauralhead over 10 years ago in reply to hiassoft

    Hello Hias,

     

    When I extract the file cirrus-linux-4.1.19.tgz (using windows PC) extract to a new folder, as the image is being extracted, the files being written from the folder "lib" - there are quite a few files (9) with the same name, but different files sizes, I get prompted to either overwrite or skip them. Not sure why there are already files written as they should all be unique. Quite confused about that!

     

    The first two are shown below.

     

    image

    image

     

    Anyway I was hoping they would be extracted so that I could then copy them to the Pi3's SD card.

     

    I'm a bit of a noob, but have several Pi's, but not had any experience with Pi2's or Pi3's though.

     

    I'm just playing with a NOOBS image that can boot the Pi3, and seeing if I can manage to get darkice to install.

     

    But any help in the mean time would be welcomed.

     

    Regards

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • hiassoft
    hiassoft over 10 years ago in reply to binauralhead

    Hi Alan!

     

    Ah, now I understand :-)

     

    You shouldn't extract the .tar.gz file on your PC, download it on your RPi and then extract it there using the commands from my webpage.

     

    sudo tar zxf cirrus-linux-4.1.19.tgz -C /

     

    sudo ensures the the command is run as root (and can overwrite the files / access the directories owned by root) and the -C / at the end ensures the files are extracted into the correct directories (/boot, /lib/modules etc).

     

    You also have to create the /etc/modprobe.d/cirrus.conf file as root, using an editor on the raspberry pi, for example using nano (that's one of the less-confusing editors on the RPi)

     

    sudo nano /etc/modprobe.d/cirrus.conf

     

    Ah, and don't forget to edit /boot/config.txt as described on my webpage.

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 10 years ago in reply to hiassoft

    Thank you for that image - I actually managed (only just before your email arrived) to do that very thing.

    I am slowly getting there, just trying to remember where the scripts were to test darkice!

     

    Not sure if any sound can be heard or recorded as yet, I've basically done it, with a reboot all seems fine (thanks to your work), just about to find the elusive scripts now, ha...

     

    Thank you so much for the work you do, though Cirrus should be doing that on OUR behalf eh..

     

    Thanks again!

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • binauralhead
    binauralhead over 10 years ago in reply to hiassoft

    Hi again,

    I resolved the darkice not starting after using aplay -l : said device = 0,0 rather than what I was using as 1,0

    Awesome, its using the on board mics at present, going to wire up for the line in for binaural audio.

     

    Warmest wishes.. you saved the day

     

    Regards

    Alan

     

    On test right now, and with luck 24/7 when the binaural microphone is connected

    http://philae.shoutca.st:8381/stream