Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Driver fixes and updates to kernel 3.18.16 and 4.0.5
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 180 replies
  • Subscribers 720 subscribers
  • Views 29151 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Driver fixes and updates to kernel 3.18.16 and 4.0.5

hiassoft
hiassoft over 11 years ago

Edit: Current kernel versions and install/config instructions are also available from my webpage http://www.horus.com/~hias/cirrus-driver.html

 

During the last few weeks I fixed various issues in the Wolfson/Cirrus driver and rebased it so it works with the current RPi kernel versions (3.18.16 and 4.0.5).

 

You can download the patches from my GitHub repository. The 3.18 kernel with Cirrus drivers is in the cirrus-3.18.y branch, the 4.0 kernel with Cirrus drivers is in the cirrus-4.0.y branch. I'll rebase and update these branches from time to time so that the Cirrus driver and my changes will stay on top of the commit list.

 

If you just want to have an updated 3.18.16 kernel you can download precompiled binaries from here. Just unpack the tarball in the root directory. Before you do that it might be a good idea to update the firmware files (bootcode.bin, start*.elf and fixup*.dat in the boot directory) to the latest version.

 

Here's a list of my changes:

- Added the FLL1 setup back so that switching between 44.1kHz and 48kHz (and other sample rates) works fine.

- Don't register Arizona IRQ if it's set to 0. The Cirrus driver uses polling here and if we register an interrupt handler for irq 0 we get lots of "spurious interrupt" messages spamming dmesg in kernel 3.19 and newer. IRQ 0 is wrong anyway.

- Include DCVDD patches from the Cirrus linux-drivers repository. These patches make sure the WM8804 chip is initialized properly. Without this patch I sometimes had SPDIF audio out only on the right channel.

- Disable spidev0 in Cirrus device tree overlay. That's mainly a safety precaution so that userspace programs trying to access spi0.0 won't interfere with the WM8804 reset line. I'm not 100% sure this is needed at all, so maybe I'll remove it some time later.

 

And some important notes:

I haven't included the mmap patch, this is already supported in the upstream kernels but currently disabled by default. To enable mmap support add the following line to config.txt:

dtoverlay=i2s-mmap

 

If you compile the kernel on your own please note that the devicetree overlays have now been moved to arch/arm/boot/dts/overlays.

 

Kernel 4.0 now uses spi_bcm2835 by default (the older spi_bcm2708 module is available via a devicetree overlay) so you have to extend your /etc/modprobe.d conf file and add a pre-depend for spi_bcm2835 as well. It's safe to have both the old and the new module in here, so just use this configuration:

softdep arizona-spi pre: arizona-ldo1
softdep spi-bcm2708 pre: fixed
softdep spi-bcm2835 pre: fixed

 

so long,

 

Hias

  • Sign in to reply
  • Cancel
Parents
  • hiassoft
    hiassoft over 10 years ago

    I've uploaded a new precompiled kernel, based on kernel 4.4.6:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.4.6.tgz

    The source code can be found here: https://github.com/HiassofT/rpi-linux/tree/cirrus-4.4.6

     

    Changes since the last version:

    • Switch to kernel 4.4 series, version 4.4.6
    • Remove now obsolete non-devicetree code from driver

     

    Important notes if you update from kernel 4.1.y:

    1. Update the GPU firmware using sudo SKIP_KERNEL=1 rpi-update before installing the 4.4 kernel. Failing to do this may result in various errors or a non-booting system!
    2. Check that you have dtoverlay=rpi-cirrus-wm5102 in your config.txt, the old variant dtoverlay=rpi-cirrus-wm5102-overlay is no longer supported.

     

    Installation and configuration instructions and troubleshooting hints can be found on my website:

    http://www.horus.com/~hias/cirrus-driver.html

     

    so long,

     

    Hias

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hiassoft
    hiassoft over 10 years ago

    I've uploaded a new precompiled kernel, based on kernel 4.4.6:

    http://www.horus.com/~hias/tmp/cirrus/cirrus-linux-4.4.6.tgz

    The source code can be found here: https://github.com/HiassofT/rpi-linux/tree/cirrus-4.4.6

     

    Changes since the last version:

    • Switch to kernel 4.4 series, version 4.4.6
    • Remove now obsolete non-devicetree code from driver

     

    Important notes if you update from kernel 4.1.y:

    1. Update the GPU firmware using sudo SKIP_KERNEL=1 rpi-update before installing the 4.4 kernel. Failing to do this may result in various errors or a non-booting system!
    2. Check that you have dtoverlay=rpi-cirrus-wm5102 in your config.txt, the old variant dtoverlay=rpi-cirrus-wm5102-overlay is no longer supported.

     

    Installation and configuration instructions and troubleshooting hints can be found on my website:

    http://www.horus.com/~hias/cirrus-driver.html

     

    so long,

     

    Hias