Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Can you program a raspberry pi using only windows?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 703 subscribers
  • Views 878 views
  • Users 0 members are here
  • raspberry_pi
Related

Can you program a raspberry pi using only windows?

e14 Contributor
e14 Contributor over 11 years ago

Been going through a bunch of Ben Heck's YouTube videos and have kinda gotten inspired to grab a couple raspberry pis to tinker with.

 

One of the things that really intrigued me was the media Centre he made with the pi. So I was wondering, is it possible to program the pi with only windows? If so, what are some things I should be getting to make it a bit easier on myself?

 

Any help is appreciated!

 

Marc

  • Sign in to reply
  • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago

    Marc Watson wrote:

     

    So I was wondering, is it possible to program the pi with only windows? If so, what are some things I should be getting to make it a bit easier on myself?

    If you want to make things easier on yourself, I suggest programming RasPi with GNU/Linux, specifically Raspbian.  The latest GUI running on a RasPi 2 is very nice IMO -- much nicer than any version of Windows I've used.  For programming, all the compilers and utilities you probably need are already in Raspbian.  All the RasPi examples and tutorials I've come across are GNU/Linux, so there's plenty of help getting started.

     

    To develop RasPi programs on Windows you need a cross-compiler.  It's called a cross-compiler because it makes you cross image  IMO it's better to stick with GNU/Linux and its happy compilers image

     

    JMO/YMMV

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • cstanton
    0 cstanton over 11 years ago

    Hello mwatson8,

     

    It depends what you mean by 'program'. If you mean create programs by writing computer code, such as in Python, C or other languages then you do not need a Windows computer to do this. It can be done either on a Linux computer or directly onto the Pi. Depending on what programming language you're using will determine if you need to cross compile, as johnbeetem suggests.

     

    If you mean 'run OpenElec' or some other operating system, then all you need is a computer with an operating system that can write an SDCard, then you just download the image, write it to the SDCard and away you go.

     

    If you're wanting to code 'baremetal' on the Pi, that's a different barrel of fun entirely.

     

    Ben Heck didn't program the Pi per say, he just downloaded an SDCard image, which I think was OpenElec (which is based on Linux) and used Win32DiskImager to write the image to the microSD Card.

     

    Does this make sense?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to cstanton

    Yes for sure, makes complete sense! I just wanted to make sure I would be able to do something with it with my current setup before I had ordered it, and with what you guys have said, I think I've got a good idea!

     

    Thanks again!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 11 years ago in reply to e14 Contributor

    Thanks mwatson8 !

    As you posted a question, be sure to mark whether people's responses were correct and/or helpful to your question image