Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi failing with camera, BMP180, and TSL2561
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 675 subscribers
  • Views 1005 views
  • Users 0 members are here
  • raspberry_pi
  • bmp180
  • tsl2561
Related

Raspberry Pi failing with camera, BMP180, and TSL2561

ttkoshi
ttkoshi over 10 years ago

Hi everyone-

 

I'm working on some sensors for a high-altitude ballooning project. I've wired together a BMP180 and a TSL2561 sensor together, and in addition added a camera and photoresistor. When I run my code in the lab, everything runs fine. However, when I am outdoors, once the sensors are off the ground, they start misbehaving. I have launched this payload twice, and twice received bad data. I have attached the graphs that were the result of the data, and you can see that there is a lot of noise from the sensors. The baseline before the changes is basically the payload sitting on the ground. In addition, the images that get taken start developing a green tint, but only once in the air. It seems my sensor is afraid of heights. I've posted the info here, as well as the code used to run it all. This is all powered by a 5V battery that returns to the ground with half charge, so I know the battery isn't being used up. I'm at my wits end, trying to find out why everything works on the ground, but not up at altitude. Other teams that I'm working with have sent up the BMP180, or a camera, but never together, I was the first to try rigging the two together. In addition, in the code you'll see that I was trying to write the altitude and temperature to the image metadata, which has worked so far. Any help would be greatly appreciated. Thank you!

 

Configuration:

- Raspberry Pi 2

- Raspberry Pi Camera

- TSL2561 Digital Luminosity Sensor (to 3.3V, reading via I2C)

- BMP 180 Temperature / Pressure sensor (to 5V, reading via I2C)

- Photoresistor (hooked to 1 microfarad capacitor) (to 5V, reading from pin 17)


#!/usr/bin/python

# Import libraries needed for program
import RPi.GPIO as GPIO, Adafruit_BMP.BMP085 as BMP085, os, datetime, time, math
from Adafruit_I2C import Adafruit_I2C

# This prevents warnings from crashing the program due to GPIO issues
GPIO.setwarnings(False)
DEBUG = 1
GPIO.setmode(GPIO.BCM)

# Define the Lux sensor and its address
address = 0x39
i2c = Adafruit_I2C(address)
control_on = 0x03
control_off = 0x00

# Initialize the BMP085 sensor in high resolution mode
sensor = BMP085.BMP085()

# Enable the Lux sensor
def enable():
   i2c.write8(0x80, control_on)

def disable():
   i2c.write8(0x80, control_off)

def getLight():
   ch0 = i2c.readU16(0xAC)    # Broad spectrum reading
   ch1 = i2c.readU16(0xAE)      # IR Reading
   return ch0, ch1

def getLux():
   ch0, ch1 = getLight()
   ratio = 0
   lux = 0
   if ch0 > 0:
      ratio = float(ch1) / float(ch0)
   if ch0 == 0:
      ratio = 1.35
   if ratio > 1.30:
           lux = 0
   elif ratio > 0.80:
           lux = (0.00146 * ch0) - (0.00112 * ch1)
   elif ratio > 0.61:
           lux = (0.0128 * ch0) - (0.0153 * ch1)
   elif ratio > 0.50:
           lux = (0.0224 * ch0) - (0.031 * ch1)
   elif ratio <= 0.50:
           lux = (0.0304 * ch0) - (0.062 * ch0 * ((ch1/ch0) ** 1.4))
   return lux, ch0, ch1

# Function to read light from photoresistor
def RCtime (RCpin):
   reading = 0
   GPIO.setup(RCpin, GPIO.OUT)
   GPIO.output(RCpin, GPIO.LOW)
   time.sleep(0.1)
   GPIO.setup(RCpin, GPIO.IN)
   while (GPIO.input(RCpin) == GPIO.LOW):
      reading += 1
   return reading

# Function to enable Lux sensor

# Main Loop
while True:
   # Assigning values to variables
   enable()
   light = getLight()
   lux, spectrum, infrared = getLux()
   now = datetime.datetime.now()
   timeStamp = now.strftime("%m%d%Y_%H%M%S")
   photoResistor = RCtime(17)
   temp = sensor.read_temperature()
   altitude = sensor.read_altitude()
   pressure = sensor.read_pressure()
   seaPressure = sensor.read_sealevel_pressure() 
   #disable()
   dataString = "Image = " + str(timeStamp) + ".jpg, Temp = " + str(temp) + ", Alt = " + str(altitude) + ", Pres = " + str(pressure) + ", SL Pres = " + str(seaPressure) + ", Photoresistor = " + str(photoResistor) + ", Lux = " + str(lux) + ", Spectrum = " + str(spectrum) + ", IR = " + str(infrared)

   # Open file for logging and record data
   logging = open('/home/pi/Code/AtmoAP/flight_data.txt','a')
   logging.write(dataString + "\n")

   # Take and save photo while embedding temp to EXIF Make and altitude to EXIT Model
   takephoto = "raspistill -md 2 -n -t 1 --exif IFD0.Make={} --exif IFD0.Model={} -o /home/pi/Code/AtmoAP/images/{}.jpg".format(str(temp),str(altitude),timeStamp)
   os.system(takephoto)
   
   #Pause
   time.sleep(2)


Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Thomas,

     

    If you're seeing corruption of image and sensors, then it is most likely something that is common to both of them - possibly power supply related or cold weather related. Perhaps the 5V (switched mode presumably) power source is dropping out when running everything, or needs supply decoupling.

    You may need to show a photo of the hardware and provide more detail of the environment for deeper examination. What battery (e.g. Li-Po?), and what temperature are you expecting to experience? Did anything else change with the successful flights, or is everything identical except that you've added more sensors?

    By photoresistor, do you mean a light dependent resistor (LDR)? What resistor value do you have in series with it? (Wondering if this is consuming too much current and pushing things into an unstable condition). How are you reading the LDR, the RPI has no analog-to-digital converter, is this some crude hack (schematic will help).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi Thomas,

     

    If you're seeing corruption of image and sensors, then it is most likely something that is common to both of them - possibly power supply related or cold weather related. Perhaps the 5V (switched mode presumably) power source is dropping out when running everything, or needs supply decoupling.

    You may need to show a photo of the hardware and provide more detail of the environment for deeper examination. What battery (e.g. Li-Po?), and what temperature are you expecting to experience? Did anything else change with the successful flights, or is everything identical except that you've added more sensors?

    By photoresistor, do you mean a light dependent resistor (LDR)? What resistor value do you have in series with it? (Wondering if this is consuming too much current and pushing things into an unstable condition). How are you reading the LDR, the RPI has no analog-to-digital converter, is this some crude hack (schematic will help).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to shabaz

    Shabaz , I agree with this troubleshooting but first of all I suggest to check the power source. I had strange behaviours and it was just the power not sufficient for all the peripherals.

     

    Enrico