Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Stepper motor control using Raspberry pi 2 and simulink
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 1083 views
  • Users 0 members are here
Related

Stepper motor control using Raspberry pi 2 and simulink

e14 Contributor
e14 Contributor over 11 years ago

I am new to the raspberry pi  and simulink. Is there a way I can write a program in simulink to control a stepper motor using raspberry pi 2. Do I need any other external circuitry other than the basic which is the stepper drive, switching  transistors, e.t.c?

  • Sign in to reply
  • Cancel
  • ravi_butani
    0 ravi_butani over 11 years ago

    Simulink support serial port...

    RPI have python lib for stepper motor and serial port...

     

    So what I suggest is generate commands from simulink and send it over serial port to RPI...

    RPI python code manipulate these command and control stepper motor from its gpio...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ravi_butani
    0 ravi_butani over 11 years ago

    For drive stepper only you need l293d and four diode or uln2003 driver Ic...no extra components needed...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rew
    0 rew over 11 years ago in reply to ravi_butani

    The ULN2003 is not suitable for most stepper motors. To use an ULN2003 as a stepper driver you need a 5-wire stepper motor. Or a 6- or 8-wire one that can be configured as a five-wire one. Many steppers are 4 wire nowadays.


    The L293D is an antique chip that could be used to drive a stepper. But certainly it won't be able to operate the stepper at close to maximum performance.


    Often there is a tradeoff where you get simplicity as a tradeoff against better performance.

     

    However in this case you can buy a "polulu stepper driver" based on say an Allegro A4988, which is simpler and will drive all steppers EXCEPT the 5-wire ones. As a bonus using that will be simpler than wiring up your own L293D stepper driver.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks guys. I found another driver that was compatible with my stepper motor, but the stepper motor however heats up quickly