Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Problems booting raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 1912 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Problems booting raspberry pi

e14 Contributor
e14 Contributor over 10 years ago

Hi,

We just received our first Raspberry Pi.  Its the latest model.  We have formatted the 8GB micro sd card including wiping any data with the Mac Disc Utility.  We have downloaded the NOOBS files, latest version, and copied them onto the sd card.  I can see them in file manager and eject the sd card correctly.  The files are copied, not the NOOBS folder.  The only folders copied are the OS and Defaults files.  However, the Raspberry pi does not boot.  Both the red power LED and the Green LED light constantly.  The Green LED does not flash at all.  I've tried without a keyboard or mouse or even a screen connected and same issue.  Any ideas of what else to try?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Unfortunately not all SD cards are the same nor work in the Raspberry Pi. Note to anyone else that may have troubles...

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to clem57

    clem57 and raspberrypimum I have also experienced that as the SD card is used almost intensively by the Linux system, if you plan to use the raspi in a project expecting it working for many hours it is the worth to invest some money to setup the external disk running as the main system after the boot (it is needed to start from the SD card and it is mandatory). There are many different solutions, from the cheap (and slow) USB memory stick up to and external USB hdd or an external USB SSD...

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to clem57

    clem57 and raspberrypimum I have also experienced that as the SD card is used almost intensively by the Linux system, if you plan to use the raspi in a project expecting it working for many hours it is the worth to invest some money to setup the external disk running as the main system after the boot (it is needed to start from the SD card and it is mandatory). There are many different solutions, from the cheap (and slow) USB memory stick up to and external USB hdd or an external USB SSD...

     

    Enrico