Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Programming for an embedded app
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 37 replies
  • Subscribers 711 subscribers
  • Views 4772 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Programming for an embedded app

e14 Contributor
e14 Contributor over 11 years ago

Background: I need to convert a 200 kHz encoder pulse train to 47.5 kHz. I tried using the Arduino Nano but it topped out at 8 kHz. Is used an ISR triggered on the rising edge of the encoder pulse and did floating point addition to determine when I should output a pulse. I know FP math in an ISR is not a good idea in general but it was simple math and the Arduino couldn't output faster than 8 kHz even w/o any ISR processing. Someone suggest using the Raspberry so I am attempting it. I have the Raspberry Pi 2 900 MHz system.

 

Main Questions:

  1. Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.
  2. I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

 

These are my main questions. I am a newbie using this and don't know all the specific steps from start to finish. I do have the Raspberry up and running but somewhat stuck after that. My internet is slow and it take forever to surf and find stuff. Is there one or two locations that can show me how to write a program from scratch. The Arduino code is less than 30 lines.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.

     

    As the Linux or Unix root (super user), edit /etc/rc.local (E.g. `su gedit /etc/rc.local`).  Just before the `exet` statement at the end of the file, this is where you will insert a command to launch whatever it is that you want launched soon after boot time.  Note that rc.local is launched just after all of the other /etc/rcN.d scripts are launched.  For more details about "rc", investigate how Linux boots and how the "init" process (pid 1) works.

     

    You probably do not want your stuff running as the root.  So, in /etc/rc.local, your command should be something like this:

     

         su -c 'COMMAND' MYUSERID

     

    where

     

         COMMAND = is the absolute path name to your shell script

         MYUSERID = the user name under which you want COMMAND to run

     

    When I do this, my shell script is always self contained i.e. I do not rely on any I/O redirection of environment variables setup for me.  Also, make sure that you check *every* exit code from any embedded executables or called scripts.

     

    Log to a directory that MYUSERID has write-access to and that will survive a reboot (E.g. do not log to /tmp).  Always include "evidence" with each log entry such process ID, date, time, and context (what was the goal?).  I would write to file names that included the date so that these log files could be aged (yes, you need to write a log-ager).

     

    I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

     

    My understanding that Windows is not yet ready for general-purpose computing on the RPi, just "IoT".  I would stick to Linux and C/C++ programming for Raspbian or one of the Ubuntu flavors.  The Gnu C/C++ compiler works very well for this purpose.  Also, there are other language options such as Java and Python which can handle GPIO.

     

    Good luck and experiment with tools.  Report back!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.

     

    As the Linux or Unix root (super user), edit /etc/rc.local (E.g. `su gedit /etc/rc.local`).  Just before the `exet` statement at the end of the file, this is where you will insert a command to launch whatever it is that you want launched soon after boot time.  Note that rc.local is launched just after all of the other /etc/rcN.d scripts are launched.  For more details about "rc", investigate how Linux boots and how the "init" process (pid 1) works.

     

    You probably do not want your stuff running as the root.  So, in /etc/rc.local, your command should be something like this:

     

         su -c 'COMMAND' MYUSERID

     

    where

     

         COMMAND = is the absolute path name to your shell script

         MYUSERID = the user name under which you want COMMAND to run

     

    When I do this, my shell script is always self contained i.e. I do not rely on any I/O redirection of environment variables setup for me.  Also, make sure that you check *every* exit code from any embedded executables or called scripts.

     

    Log to a directory that MYUSERID has write-access to and that will survive a reboot (E.g. do not log to /tmp).  Always include "evidence" with each log entry such process ID, date, time, and context (what was the goal?).  I would write to file names that included the date so that these log files could be aged (yes, you need to write a log-ager).

     

    I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

     

    My understanding that Windows is not yet ready for general-purpose computing on the RPi, just "IoT".  I would stick to Linux and C/C++ programming for Raspbian or one of the Ubuntu flavors.  The Gnu C/C++ compiler works very well for this purpose.  Also, there are other language options such as Java and Python which can handle GPIO.

     

    Good luck and experiment with tools.  Report back!