Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Programming for an embedded app
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 37 replies
  • Subscribers 711 subscribers
  • Views 4772 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Programming for an embedded app

e14 Contributor
e14 Contributor over 11 years ago

Background: I need to convert a 200 kHz encoder pulse train to 47.5 kHz. I tried using the Arduino Nano but it topped out at 8 kHz. Is used an ISR triggered on the rising edge of the encoder pulse and did floating point addition to determine when I should output a pulse. I know FP math in an ISR is not a good idea in general but it was simple math and the Arduino couldn't output faster than 8 kHz even w/o any ISR processing. Someone suggest using the Raspberry so I am attempting it. I have the Raspberry Pi 2 900 MHz system.

 

Main Questions:

  1. Is it possible to booth the system and auto load an executable w/o having to login? I want it to run like an embedded system.
  2. I want to write the code in my MS Visual C environment. How do I compile it for running on the Raspberry. Do I copy the code on to the SD card and compile and run on the Raspberry?

 

These are my main questions. I am a newbie using this and don't know all the specific steps from start to finish. I do have the Raspberry up and running but somewhat stuck after that. My internet is slow and it take forever to surf and find stuff. Is there one or two locations that can show me how to write a program from scratch. The Arduino code is less than 30 lines.


  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    As to the first question, Bob Alexander answered this one and I agree. The second one depends where the MS Visual C environment is running. If on a PC, then you cannot because it relies on DLL's that are not compiled to run on ARM code for Raspberry Pi. If on the other hand, it is on Windows 10 2015 Visual C++ built for cross compiling for Raspberry Pi and the Pi runs Windows 10 (whew), the answer is yes. I agree that GCC (free as in beerimage) is a great alternative as stated above.

    C

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 11 years ago

    As to the first question, Bob Alexander answered this one and I agree. The second one depends where the MS Visual C environment is running. If on a PC, then you cannot because it relies on DLL's that are not compiled to run on ARM code for Raspberry Pi. If on the other hand, it is on Windows 10 2015 Visual C++ built for cross compiling for Raspberry Pi and the Pi runs Windows 10 (whew), the answer is yes. I agree that GCC (free as in beerimage) is a great alternative as stated above.

    C