Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Maximum pins that can be used for i/o in RaspberryPi2 J8 header?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 1331 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
Related

Maximum pins that can be used for i/o in RaspberryPi2 J8 header?

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I am planning to use Raspberrypi2 for making a hardware. I am using Rpi2 as the processing part. I need 27 pins to be interfaced. I see that there are 17 gpio pins on the J8 header.

My question is can I use spi and i2c pins as input/output pins? Also the reserved pins can be used for i/o?

 

Regards,

Hidayat

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    if you do not need really high speed then you can use a SPI port expander like the 23S17, this is the one used on a PiFace Digital II and the newer version of it that is stackable

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    if you do not need really high speed then you can use a SPI port expander like the 23S17, this is the one used on a PiFace Digital II and the newer version of it that is stackable