Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum OBDII USB device kills UART GPS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 705 subscribers
  • Views 756 views
  • Users 0 members are here
  • raspberry_pi
Related

OBDII USB device kills UART GPS

e14 Contributor
e14 Contributor over 10 years ago

HI I have been trying to setup a car PC using the Raspberry Pi 2, and have run into a problem which i have been unable to solve with my limited knowledge of Linux.

 

I have a UART GPS connected to the GPIO pins which works fine (get data from gps with cgps -s) until I plug in my USB OBDII device, as soon as I plug it in and reboot I no longer get any data from the GPS (cgps -e Error: GPS timeout).

 

Other post I have seen suggest that its a power issue. I have eliminated this as the problem by running the Pi on a separate power supply to the powered USB HUB that the USB OBDII device is connected to. (Both power supplies are capable of delivering up to 5Amps).


Some more info..

 

With OBDII USB device disconnected I ran gpspipe -r and got DEVICE path = /dev/ttyAMA0 as expected..

 

When I connected the OBDII USB device and ran gpspipe -r I got DEVICE path = /dev/ttyUSB0..

 

Hope this will help someone give me a solution.

 

In etc/default/gpsd DEVICE is listed as dev/ttyAMA0

 

Im guess that this is what the problem is, I would like to know why it switches to ttyUSB0 when the OBDII USB device is connected.

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 10 years ago

    Sounds like your gpspipe program is picking up the wrong device in error.

    You could force gpspipe to use the correct device on the command line according to here:

    http://www.catb.org/gpsd/gpspipe.html

     

    Isn't the last parameter the device name? i.e. you could type :/dev/ttyAMA0 on the end of your command line, or something like that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thanks for the info I tried gpspipe -w :/dev/ttyAMA0 with error could not connect to gpsd localhost:/dev/ttyAMA0, Unknown error 4294967294(-2)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    Hi John,

     

    Looks like I got the command wrong : (

    I've never used this before. Anyway, looks like 'gpsd' is the program which gpspipe is connecting to. And gpsd I suspect is using the wrong device.

     

    Could you check what runs gpsd in your solution (i.e. it could be a script) and the command line for it allows you to specify the device name, i.e. /dev/ttyAMA0 according to this page http://www.catb.org/gpsd/gpsd.html

    (snippet:)

    Arguments are interpreted as the names of data sources. Normally, a data source is the device pathname of a local device from which the daemon may expect GPS data. But there are three other special source types recognized, for a total of four:

    Local serial or USB device

    A normal Unix device name of a serial or USB device to which a sensor is attached. Example: /dev/ttyUSB0.

    .....