Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry PI 2 or Compute module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 709 subscribers
  • Views 3703 views
  • Users 0 members are here
  • compute_module
  • ethernet
  • embedded_os
  • io_module
  • raspberry-pi
  • raspberry_pi_space
  • development_kit
  • display
  • custom_solution
  • raspbian
  • real-time_operating_system
Related

Raspberry PI 2 or Compute module

balearicdynamics
balearicdynamics over 11 years ago

Unfortunately this is not a tutorial nor a specific question; I'd like start a discussion to all the users that are interested and those that - hopefully - has a minimum of experience on the use of the Raspberry PI compute module.

 

My starting point, as far as I know and read here and there in the documentation is a bit confusing and can be synthesised as follows:

 

  • The compute module is the "core" of a raspberry PI, probably equivalent to a B+ 512 Mb Ram and in the DIMM memory size it includes ... just only the processor and the flash memory + RAM
  • There is a very good kit that can host the computer module exposing all the GPIO, interfaces, camera, display etc. But the resulting price, without the ethernet connection and a couple of other secondary components, is about the double of a Raspberry PI2 (that is the next PI version, faster, more memory etc.
  • Any customer can develop its own I/O board saving money, but the Computer module alone is not sold. So the only possibility is to buy the entire kit
  • It is presented like the "pro" version of the Raspberry PI for industrial applications and more sophisticated embedded developments, but has less things and my perception is that is less flexible.
  • In some documents it is explained that it can be designed to support pre-built cstomer programs developed under Linux all flashed on the module, but in some other documentation are mentioned pay-per-license operating systems.

 

These are only some of the incongruences that it seems emerging from the first view comparison. In a project I am working with I though about the computer module as an alternative to the PI but to be honest I have a lot of perplexity.

 

I hope that someone explain me that I am totally wrong, I have not understood the basic principle and tell me what is the reason to make this choice creating a custom system running a bunch of specific applications. And also what can be the reason of a so high (double) price that makes this device IMHO absolutely not competitive respect the Raspberry PI 2.

 

Enrico

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    Jumping in late: My understanding is that the Compute Module happened because people said they wanted to use RasPi in actual products but didn't want to mess with the nasty original Model A/B form factor with connectors on all four sides.  Plus they wanted more GPIOs than the original Model A/B, and something that used less power.

     

    So to satisfy all these requirements in the most flexible way, you get the Compute Module.  Unfortunately, a modular design is always more expensive than a single-board design: you have more connectors and more PC boards.  Sure, you can snap things together like Lego, but Lego is expensive too.

     

    I suspect that once people saw the price, the demand evaporated and they either kludged the existing board or did a fully-custom design with a different SoC.

     

    The other thing that happened is that the B+ came out a couple months after the Compute Module.  The B+ added GPIOs and replaced the inefficient LDO voltage regulators with switchers.  So RasPi itself eliminated two of the reasons for the Compute Module.

     

    Update:  The Model A+ was another nail in the Compute Module coffin.  If you can get by with 256MB DRAM, the Model A+ gets you a RasPi with single USB for US$20.  You can then plug in your own USB expansion board designed for your product and/or pop on a custom HAT.

     

    JMO/YMMV

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago

    Jumping in late: My understanding is that the Compute Module happened because people said they wanted to use RasPi in actual products but didn't want to mess with the nasty original Model A/B form factor with connectors on all four sides.  Plus they wanted more GPIOs than the original Model A/B, and something that used less power.

     

    So to satisfy all these requirements in the most flexible way, you get the Compute Module.  Unfortunately, a modular design is always more expensive than a single-board design: you have more connectors and more PC boards.  Sure, you can snap things together like Lego, but Lego is expensive too.

     

    I suspect that once people saw the price, the demand evaporated and they either kludged the existing board or did a fully-custom design with a different SoC.

     

    The other thing that happened is that the B+ came out a couple months after the Compute Module.  The B+ added GPIOs and replaced the inefficient LDO voltage regulators with switchers.  So RasPi itself eliminated two of the reasons for the Compute Module.

     

    Update:  The Model A+ was another nail in the Compute Module coffin.  If you can get by with 256MB DRAM, the Model A+ gets you a RasPi with single USB for US$20.  You can then plug in your own USB expansion board designed for your product and/or pop on a custom HAT.

     

    JMO/YMMV