Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB POWER BANK // PORTABLE POWER SUPPLY
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 5383 views
  • Users 0 members are here
  • power
  • bank
Related

USB POWER BANK // PORTABLE POWER SUPPLY

e14 Contributor
e14 Contributor over 10 years ago

Hi, I got me a raspberry pi 2 model B with UK power standards. Have anyone power this device with a usb power bank that is for charging a smartphone?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

     

    Nod* default 5v usb 2.0 that draws from a PC

     

     

     

    I thought “atleast 700mAh” is not more than that, but it’s a mod discussion right..but still im afraid to do this mod..heh. Great and easy to understand on the PC USB explanation. Thanx

     

     

     

    Does that mean a power source more than 700mA is safe for the pi2mB?

     

     

     

    I tested a 2-in-1 desktop charger that charges Li-ion 1320mAh battery for a phone that can be a power bank as well, when the battery is fasten to the charger. The USB port output 5.2V 800mA

     

     

     

    I tested this on my phone 600 MHz Cortex-A8 which feeds DC 5.0V/1200mA to support my thoughts about pi2mB USB current, I did a cold boot on my phone, but wasn’t enough it only last for less than 20-30 sec then powers down. This could be the charger is not drawing enough current. Will testing this on pi2mB safe?

     

    I tested the phone with the 2 usb ports 1)1A 2)2.1A of the power bank and both port testing 1 by 1  charges the phone, and this smartphone has a built in charging script if it is not enough power it will prompt me a message and its built for a usb powerbank right?

     

     

     

    Does pi2mB have a voltage regulator? Because I saw a vid this person was using an additional board for voltage regulator on his pi1 don’t know if its model B or the default pi1 model, then power it up with a power bank.

     

     

     

    Will this be the same result as with pi2mB? Meaning without an extra board with regulator

     

     

     

    I did a mod from a PSU 12v DC to power a small car air compressor that feeds from a cigarette lighter power slot, changed it, so that I can use the house power outlet with a 3 pin plug, without knowing its mAh it worked this was because it’s a really direct current.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

     

    Nod* default 5v usb 2.0 that draws from a PC

     

     

     

    I thought “atleast 700mAh” is not more than that, but it’s a mod discussion right..but still im afraid to do this mod..heh. Great and easy to understand on the PC USB explanation. Thanx

     

     

     

    Does that mean a power source more than 700mA is safe for the pi2mB?

     

     

     

    I tested a 2-in-1 desktop charger that charges Li-ion 1320mAh battery for a phone that can be a power bank as well, when the battery is fasten to the charger. The USB port output 5.2V 800mA

     

     

     

    I tested this on my phone 600 MHz Cortex-A8 which feeds DC 5.0V/1200mA to support my thoughts about pi2mB USB current, I did a cold boot on my phone, but wasn’t enough it only last for less than 20-30 sec then powers down. This could be the charger is not drawing enough current. Will testing this on pi2mB safe?

     

    I tested the phone with the 2 usb ports 1)1A 2)2.1A of the power bank and both port testing 1 by 1  charges the phone, and this smartphone has a built in charging script if it is not enough power it will prompt me a message and its built for a usb powerbank right?

     

     

     

    Does pi2mB have a voltage regulator? Because I saw a vid this person was using an additional board for voltage regulator on his pi1 don’t know if its model B or the default pi1 model, then power it up with a power bank.

     

     

     

    Will this be the same result as with pi2mB? Meaning without an extra board with regulator

     

     

     

    I did a mod from a PSU 12v DC to power a small car air compressor that feeds from a cigarette lighter power slot, changed it, so that I can use the house power outlet with a 3 pin plug, without knowing its mAh it worked this was because it’s a really direct current.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer