Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum win32diskimager not enough space
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 5276 views
  • Users 0 members are here
Related

win32diskimager not enough space

vindhyachal.takniki@gmail.com
vindhyachal.takniki@gmail.com over 10 years ago

1. I have a 8gb sd card with raspian image. Also I had expanded filesystem using sudo raspi-config.

2. After that I had crated image using win32diskimager. Image size is around 8,068,792,320 bytes .

However when I try to burn same image back to same sd card, win32imager shows error that not enough space.

3. Strange thing is sd card is same, same image is read , but when I write back it fails.

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 10 years ago

    Um do you have a Linux install you can use ?

    In that case you can use "dd" to create and write the saved image.

    You shouldn't get the same problems reading and writing even if something is "shorter" , I suspect that the program is appending some data to the end to pad it out !

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 10 years ago

    Um do you have a Linux install you can use ?

    In that case you can use "dd" to create and write the saved image.

    You shouldn't get the same problems reading and writing even if something is "shorter" , I suspect that the program is appending some data to the end to pad it out !

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to Problemchild

    John is on the correct path. See SD Image won't fit on SD Card - Raspberry Pi Stack Exchange which explains in more detail. The problem is data can be deleted yet still exist on the card. Win32diskimager will copy even this. Note you expanded that as well using sudo raspi-config. This creates the largest possible file system. That could create some padding at the end that Linux can handle. But Windows utility cannot realize and wants to allocate them causing just a bigger image. The answer is to shrink. BTW, did you reformat the card? This could change the sector size and indicate less room than before. Try to reformat with 512 byte sector. Contrary to what may be expected, a 1024 may have better fit. The logic here is the space between sectors is fixed and wasteful. So fewer spaces is better to some degree.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to clem57

    Clem, sector size on modern Multi level flash chips is 4k. In the old days with single level cells, you'd have most sectors containing about 0 errors. Then there was the ECC that could correct the occasional bit flip and even two or three flipped bits just to be sure.

     

    However, modern MLC chips end up with an average of around 4 bit flips for every sector (on the one chip where I tested all this) . To reliably fix that, you need a much bigger amount of ECC. Increasing the sector size, with the proper ECC will improve reliabilty. If you start out with say x bytes of ECC per 512byte block and then move to 2x bytes for a 1024 byte block, if the original could fix 10 bit flips then the 2x bytes in a 1024 byte block will be able to handle almost 20 bit flips. So the bigger chunk can easily handle say 15 bit flips, even when they are all in the first 512byte block, while the original could only handle 10 bit flips in any one sector.

     

    So, physical sector sizes are 4k nowadays. Both on harddrives and SD cards.

     

    All this ECC stuff is hidden from the computer at the SD card interface. There is no way you can "format" an SD card with 512 or 4096 byte sector size from the computer. The SD card presents "an array of 512 byte sectors" to the PC. Even if the internal physical structure has 4k sectors the standard requires it to handle 512byte blocks.