Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Multilevel Temperature control
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2806 views
  • Users 0 members are here
  • python
  • raspberry_pi
Related

Multilevel Temperature control

terryaris
terryaris over 10 years ago

I would like to control oven temperature with a Raspberry Pi.  I have a simple on-off control with deadband working well now.  My challenge is I need to control the oven to different temperatures for different time periods:  ie:  0 to 200F over a period of 6 hrs, cool to 125F over a period of 4 hrs, then back to 280F for 3 hrs.  I hope to do this with a while loop but do not really understand how to proceed once my first setpoint and time has completed.  I will count down the time with the time function, so once the first one zeros out, how do I proceed to the next setpoint/time ramp for the cooling phase?  Any suggestions or if you could direct me to some code that is already built it will be great! 

  • Sign in to reply
  • Cancel
  • mconners
    0 mconners over 10 years ago in reply to terryaris

    Seems like it was more Roger than me. He provided the meat of the solution. I just gave some OS pointers. Glad it worked out for you.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to mconners

    BTW, if you ever type

     

    ls -al

     

    you see something like

     

    drwxr-xr-x  4 mconners mconners 4096 Feb 12  2015 .

    drwxr-xr-x 14 mconners mconners 4096 Nov 20 13:53 ..

    -rw-r--r--  1 mconners mconners  553 Feb 12  2015 foo.cs

    -rwxr-xr-x  1 mconners mconners 3584 Feb 12  2015 foo.exe

     

    the first character  d indicates that it is a directory

    . is the current directory

    .. is the parent directory

     

    -rw-r--r-- means  that the file is read/write for the owner,read only by the group, and read only for world (everyone else)

    -rwx-r-xr-x means read/write/execute for the owner, read/execute for the group, and read/execute for the world

     

    this pattern of rwx can be set on a file using the chmod command, where each set of rwx is an octal digit

    so 755 = 111 101 101

    which translates to rwx r-x r-x

     

     

    so that's what the chmod 755 did

    and the ./program means execute program in the current directory

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to mconners

    Mike,

    You're going too fast with the binary stuff.

     

    On chmod you specify three digits. FIrst is for owner, second for group, third for others. Common values are: 6 for "read-write". and 4 for "readonly". when the file is a program that is executable, the numbers are 7 for read/write (and execute) and 5 for read-only (and execute).

     

    This leads to the following common combinations. 644: read/write for the owner, and readonly for group and others.

    Or 664 for read/write for owner and group, readonly for others.


    For executable programs those combinationsbecome 755 for only owner can write and 775 for group can write as well.

    On "ls" the 644 is shown as rw-r--r--, 664 is shown as rw-rw-r--, 755 is shown as rwxr-xr-x and 775 is shown as rwxrwxr-x.

     

    I'm not going to tell you that some people ignore the rules and specify 4 digts to "chmod": 4755.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 10 years ago in reply to rew

    Yeah, you might be right, Roger. I do that sometimes.image At least I didn't tell him about the extra bits like you did. image

     

    Between the 2 of us, I think we have it covered.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terryaris
    0 terryaris over 9 years ago in reply to rew

    Roger:

    Subject: Re: [Raspberry Pi] - Multilevel Temperature control

    Hello Roger, you once helped me out with temperature control on my malting operation here in Ecuador. I have that part of the system up and running well now but have upped the anti a bit, and need to go to some higher temperatures - ie 400F which is above the limit of my DS18B20. I have managed to find a MAX6675 K type TC unit here, only to discover that it is obsolete, giving me a challenge finding info for setting it up to read these higher temperatures. Is it possible to get the library and possibly the code for this unit or am I just out of luck?

     

     

    Can the library for the MAX 38155 be used with the MAX6675 to get some sort of readout?

    Thanks for any info you may be able to supply. 

    Terry Aris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • terryaris
    0 terryaris over 9 years ago in reply to mconners

    Subject: Re: [Raspberry Pi] - Multilevel Temperature control

    Hello Mike, you once helped me out with temperature control on my malting operation here in Ecuador. I have that part of the system up and running well now but have upped the anti a bit, and need to go to some higher temperatures - ie 400F which is above the limit of my DS18B20. I have managed to find a MAX6675 K type TC unit here, only to discover that it is obsolete, giving me a challenge finding info for setting it up to read these higher temperatures. Is it possible to get the library and possibly the code for this unit or am I just out of luck?

     

    h

    Can the library for the MAX 38155 be used with the MAX6675 to get some sort of readout?

    Thanks for any info you may be able to supply. 

    Terry Aris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mconners
    0 mconners over 9 years ago in reply to terryaris

    here is an Arduino library for the 6675

     

    https://github.com/adafruit/MAX6675-library

     

    and here is some code using wiring pi

     

    WiringPi for Raspberry Pi and MAX6675 thermal-couple sensor

     

    I'm not familiar with either of these modules, so I can't really help you there. They were just what came up when I googled

    MAX 6675 library

     

    I also don't have a 6675 so I can't really help debug them.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to terryaris

    Hi Terry,

    Good to hear that it works. :-)

     

    I have a little project with a MAX38155. I have not looked into the compatiblity with the older 6675 chips.

     

    But Maxim is inclined to keep the protocols the same as much as possible. Many people who for example know the 6675 chip, will decide: "We can just as well use the TI chip instead of the Maxim one, if we have to rewrite the software". So Maxim is interested in keeping the protocol the same. "only minor changes" or "no changes at all".
    So find the datasheets and try to see for yourself if they are the same. After you've made a decision, you're welcome to post again including your verdict and with links to both datasheets. Then it's easy for me to verify your claim.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<