Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is my raspberry unrepairable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 64 replies
  • Answers 2 answers
  • Subscribers 714 subscribers
  • Views 11904 views
  • Users 0 members are here
  • raspberry_pi
Related

Is my raspberry unrepairable?

e14 Contributor
e14 Contributor over 10 years ago

First of all I'm a beginner, so please don't judge me I know I did something bad.

 

SO, yesterday I was trying to make my raspberry pi 2 B to work with an external battery. I took a lithium polymer battery with 3.7v and 2500mah and I connect it to a booster. At first I was trying to hook it up to the micro usb input on the board and it didn't work. Then I look in youtube and I saw people plugging external batteries into the gpio pins. I joined the positive cable into the the first 5v pin and the negative cord into the first 3.3v pin and vs. Although when I connected the positive cable into the first 5v pin and the negative into the 3.3v pin for the second time with longer time touching them, it sparked and then I saw it left a kind of cut in both gpio pins. Now this morning that I try to power up my raspberry with a normal micro usb cable, I can feel the board getting warm(normal warm) but the led does not turn on.

 

In the pictures attached, the voltmeter says 4.12 v output but yesterday I adjust it to 5.2v also using the voltmeter but I don't know why it shows 4.12v now... And also in the mark on gpio is the same in the other side (the first 3.3v pin).

 

Is there anything I can do? Or is it burnout forever?

 

Thanks in advance.

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You have most lightly blown something on the PI

     

    The 4.3V battery should NOT have been connected between the 3.3V pin and the 5V pin, these are both seperate power + rails for parts of the PI board and you just put effectivly 8V into the 5V pin or caused excessive current to flow through pins not designed to have a difference of the battery or booster voltage.

     

    What you should have done is connect the batter or booster output to 0V for the black wire and 5V for the red one (Using the booster to give you the 5V

     

    you best option is actually to feed the 5V into the PI via the USB connection though, so battery to booster, booster to PI USB power connector

     

    the schamatics have not been published but based on your description of how you connected a battery capapable of providing many amps between the 3V3 and 5V pins I would expect something to have failed

     

    Sorry for the bad news, may the PI RIP.

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    So I cannot replace anything (nothing has physical damage except the pins, so I thought I may be able to replace them or even replace the led xd)? And one more question how can I put the black cable to 0v (because both cable where fused with the + and - of the boost output) ?

     

    Thank for the fast responding! :O

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    You're welcome!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bodgy
    0 bodgy over 10 years ago in reply to e14 Contributor

    --

     

    colin@btech-online.co.uk

     

    Web presence: www.btech-online.co.uk

     

    Hosted by:  www.justhost.com.au

     

    This email is to be considered private if addressed to a named 

    individual or Personnel Department, and public if addressed to a blog, 

    forum or news article.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bodgy

    ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bodgy
    0 bodgy over 10 years ago in reply to e14 Contributor

    Sorry, I don't know what went wrong with my email there.

     

    What you need is a resistor ideally around 5 ohms rated at 5 watts or more, this will test your booster at the full output (I'm assuming your booster can provide around 1 amp). You connect it between the positive and zero volts connections at the output of the booster. Then get your multimeter and measure the voltage by placing the multimeter leads on either side of the resistor.

     

    You might have made a mistake when you first set up your meter, as setting it to the 20V DC range should show be fine. Make sure you have turned it to the DC measurement range as you will get strange readings if set to the AC.

     

    You could use a higher value resistor, but as you increase the value of the resistor the amount of current drawn from the power supply will go down. This can be important, as the booster might work fine at low currents and show around 5V, but as more current is needed by whatever it is connected to the voltage will drop considerably if the booster is faulty. Which is why you should try to test the booster near to the maximum current it might need to provide.

     

    Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to bodgy

    To substantiate Collins point about testing under load... A friend dropped by yesterday evening and asked me why his system didn't work. He has a DCDC converter (actually two) set for 13.6V, but they dropped to 10V under the intended load. (one always did so immediately, the other would sometimes hold out at 13.6V for a short while before dropping).

     

    @Colin: resistors can be used outside their stated wattage without problems. In an experiment last week I needed a load for a 20V system. So grabbed the "cheap resistors" bag and the first one I pulled out was 100 ohms. 20V/100Ohms  = 200mA. That'll be fine for testing at first. But 200mA * 20V = 4W. So I grabbed 4 of the resistors, twisted them into 2S/2P configuration for quadruple the wattage = 4*0.25=1W. I'll stay below 1W by PWMing the thing at most 25%... Well you know how things go. When PWMing at 25% works you work your way up to 90 or 100%. Then you get the smell of burnt-electronics. Darn! Blew something up anway? Nope, just the resistors getting a tan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    I friend of mine did a similar mistake with its Pi. We unsoldered the switching regulator chip and the reset chip. Then, using a 1.8V LDO and a lab power supply set for 3.3V, we powered the 1.8V and the 3.3V rails of the board. We were amazed to see the processor and memory were still in working condition. You might try this approach as a last hope. Good luck

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to bbolo1

    Hi!

     

    Just wondering, is there a particular website that was followed that caused the issue? Perhaps that site is not doing a good job explaining exactly where to connect the signals. There are plenty of websites with poor (and incorrect) information unfortunately. Or could just be user error I guess.

     

    But, as you say, there is a chance to get it functioning with this method. A bit difficult for a beginner though, who may never have used an LDO or lab supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 10 years ago in reply to shabaz

    In my friend's case, it was a plain mistake. He had the correct header pinout designations printed out, however he didn't focused and he connected the wrong pins for the power supply.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Thank you for the idea! I'll try it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Hi! Can a normal battery with a volts regulator be used instead of the lab power supply?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Hi! Can a normal battery with a volts regulator be used instead of the lab power supply?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    Yes, if the battery capacity has at least a few hundreds of mAh. You need to use LDOs for all the power supply rails needed by the Broadcom CPU.

    Unfortunately, as far as I know there's no available schematic for RPi 2. The schematics for the older boards are available but in order to be able to see if yours is still in working condition, you will need a working board to get some correct voltage measurements as reference. I can take mine tomorrow and measure the voltage in a few key places.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    If you are plugging in a standard 5V 1A ish adapter to the USB power port and it is not powering up then its a pretty good bet it wont and something is fried based on the previous descriptions

     

    At the end of the day it does not matter where the power comes from, if your feeding the right volts to the USB port and its not working then it is a conformation it is dead.

     

    This assumes the power supply is good and the SD card is still functional (It too caould have been blown during the mix up of the power connections)

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Yes pleas!!!! But first, is the "AMS1117-1.8V 3pins voltage regulator SMD chip LDO transistor 1.8v" a good one for the experiment?  Thanks!!