Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is my raspberry unrepairable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 64 replies
  • Answers 2 answers
  • Subscribers 714 subscribers
  • Views 11943 views
  • Users 0 members are here
  • raspberry_pi
Related

Is my raspberry unrepairable?

e14 Contributor
e14 Contributor over 10 years ago

First of all I'm a beginner, so please don't judge me I know I did something bad.

 

SO, yesterday I was trying to make my raspberry pi 2 B to work with an external battery. I took a lithium polymer battery with 3.7v and 2500mah and I connect it to a booster. At first I was trying to hook it up to the micro usb input on the board and it didn't work. Then I look in youtube and I saw people plugging external batteries into the gpio pins. I joined the positive cable into the the first 5v pin and the negative cord into the first 3.3v pin and vs. Although when I connected the positive cable into the first 5v pin and the negative into the 3.3v pin for the second time with longer time touching them, it sparked and then I saw it left a kind of cut in both gpio pins. Now this morning that I try to power up my raspberry with a normal micro usb cable, I can feel the board getting warm(normal warm) but the led does not turn on.

 

In the pictures attached, the voltmeter says 4.12 v output but yesterday I adjust it to 5.2v also using the voltmeter but I don't know why it shows 4.12v now... And also in the mark on gpio is the same in the other side (the first 3.3v pin).

 

Is there anything I can do? Or is it burnout forever?

 

Thanks in advance.

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You have most lightly blown something on the PI

     

    The 4.3V battery should NOT have been connected between the 3.3V pin and the 5V pin, these are both seperate power + rails for parts of the PI board and you just put effectivly 8V into the 5V pin or caused excessive current to flow through pins not designed to have a difference of the battery or booster voltage.

     

    What you should have done is connect the batter or booster output to 0V for the black wire and 5V for the red one (Using the booster to give you the 5V

     

    you best option is actually to feed the 5V into the PI via the USB connection though, so battery to booster, booster to PI USB power connector

     

    the schamatics have not been published but based on your description of how you connected a battery capapable of providing many amps between the 3V3 and 5V pins I would expect something to have failed

     

    Sorry for the bad news, may the PI RIP.

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    So I cannot replace anything (nothing has physical damage except the pins, so I thought I may be able to replace them or even replace the led xd)? And one more question how can I put the black cable to 0v (because both cable where fused with the + and - of the boost output) ?

     

    Thank for the fast responding! :O

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    That is probably fine, but might be worth testing it before you connect it to anything. You need a multimeter to see if it gives 5V.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Before I joined the cables to the gpio pins, I adjusted the booster to 5.2v but after, the next day, I retest it and it showed 4.12v output.. this means it got affected?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    If its behaviour has changed then yes. Not all have protection. Anyway you have to use your own judgement and experimentation here, since I'm speculating. If you're measuring 4.2v when it was originally 5 or 5.2V then all other things being equal it looks like a fault.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    alright, Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Understood Shabaz - Thanks, much!

     

    I was trying to give him general reasons how/why things fail.  I know something of the circuitry in the RPi, but certainly not that much.  Thanks for the insight!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 10 years ago in reply to shabaz

    shabaz wrote:

     

    That is probably fine, but might be worth testing it before you connect it to anything. You need a multimeter to see if it gives 5V.

    To be really sure you should test the regulator under load (a resistor of a few watts will do) to test that the regulator does indeed deliver the current at the voltage specified even under a realistic load

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Problemchild

    Huhhhh.... image I don't get it. I should buy a resistor and connect it to the booster (including the battery) and then I should test the volts ? I'm confused how I'm supposed to know if it works cuz first time I bought it, I connected my voltmeter(at 20v) to the the output and it showed 1. So, I lower it until it says 5.2v. But what am I supposed to see now if it works, it has to say 1 again? Or put it more higher the voltmeter and see a specifc number ? And also do any resistor work or is there an especific one ?

     

    thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    Hi Mauricio,

     

    John is saying that your boost converter needs testing, and that to test it you can use a resistor (see ohms law on wikipedia) to confirm it can support the 1A or so the pi may need. If you've bought some low-cost boost converter from eBay then it may need testing basically. Another option is a ready-made battery pack intended for charging mobile phones. It has a built in battery and boost converter and is a fixed voltage - no need for any adjustments. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to shabaz

    Maricio: I have measured one of my converters (I don't remember if it was a net-power adapter, a boost or a buck converter) to increase voltage if the output current goes up. This compensates a bit for the losses is bad cables, but if you're using good ones, the 5.2V may increase too much. So... that needs checking....

     

    That said: The 'pi should work from the battery voltage directly. It's just that peripherals like USB mouse and HDMI->VGA converters are more picky about the voltage....

     

    The "under load" that was proposed should be about "1A", so with ohms law we calculate 5V/1A = 5 Ohms. At 1A and 5V the power is 5W. Normally I would recommend that you use a resistor with a higher rating than strictly necessary. In  this case 10W. But if you restrict your testing to say a few minutes, a 5W or even 2.5W model will do. Just don't leave it "testing" overnight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    If I understood I have to plug the convector with a resistor of 5w-10w and test the amperes and it has to be 1A?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    If I understood I have to plug the convector with a resistor of 5w-10w and test the amperes and it has to be 1A?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    If you can find a 5 ohm resistor, Ohms law will hold. If you measure the voltage, you can calculate the current. But measuring the current would be fine too.

     

    Actually, the voltage is way more important. You want the adapter to deliver 5V EVEN when the current is 1A. So: trust the resistor to draw "about 1A" when you connect it, and then check the voltage.

    If you can order at farnell:

    CP00105R000JE14 - VISHAY DALE - Through Hole Resistor, CP Series, 5 ohm, 10 W, ± 5%, Axial Leaded | Farnell element14

    is a matching resistor. If you want to save about half a euro, MCKNP03UJ050JB00 - MULTICOMP - Through Hole Resistor, MCKNP Series, 5 ohm, 3 W, ± 5%, 500 V, Axial Leaded | Farnell elem… will last long enough for the experiment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    Thank you!!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Mauricio;

     

    What John and Shabaz are saying is that you have to put your boost converter (or anything that supplies power: an actual power supply, buck/boost converter, transformer, etc.) under load (connect them into something that actually uses the power).  This can be a resistor (this is great as you know what the resistance is) or any kind of "black box" that uses a known combination of any two: voltage, current, or resistance.  It depends upon what the unknown is.  If you don't know current, you want to use a known voltage and resistance, for unknown voltage you use known current and resistance, for unknown resistance you use known current and voltage.  These are just the algebraic permutations of Ohm's Law: voltage=current x resistance (E=IR or V=IR, depending upon how you were taught).

     

    I've got several nominal 12V/2A switching power supplies that are 15-16V without a load.  They drop to 11.8-12.5V under a minimum 220ohm load.  You won't get reliable measurement of what your power source is doing without putting it in the same conditions as expected when it's operating.  I once had a nominal 20VDC power converter that I didn't test - Just took the manufacturers specs.  It was at 28VDC with no load.  When I plugged the hot power supply into my circuit there was enough juice to let the magic smoke out of my 25V filter cap before the voltage dropped to the rated level.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thank for the clarification :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    You're welcome!