Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is my raspberry unrepairable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 64 replies
  • Answers 2 answers
  • Subscribers 714 subscribers
  • Views 11918 views
  • Users 0 members are here
  • raspberry_pi
Related

Is my raspberry unrepairable?

e14 Contributor
e14 Contributor over 10 years ago

First of all I'm a beginner, so please don't judge me I know I did something bad.

 

SO, yesterday I was trying to make my raspberry pi 2 B to work with an external battery. I took a lithium polymer battery with 3.7v and 2500mah and I connect it to a booster. At first I was trying to hook it up to the micro usb input on the board and it didn't work. Then I look in youtube and I saw people plugging external batteries into the gpio pins. I joined the positive cable into the the first 5v pin and the negative cord into the first 3.3v pin and vs. Although when I connected the positive cable into the first 5v pin and the negative into the 3.3v pin for the second time with longer time touching them, it sparked and then I saw it left a kind of cut in both gpio pins. Now this morning that I try to power up my raspberry with a normal micro usb cable, I can feel the board getting warm(normal warm) but the led does not turn on.

 

In the pictures attached, the voltmeter says 4.12 v output but yesterday I adjust it to 5.2v also using the voltmeter but I don't know why it shows 4.12v now... And also in the mark on gpio is the same in the other side (the first 3.3v pin).

 

Is there anything I can do? Or is it burnout forever?

 

Thanks in advance.

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • gregoryfenton
    0 gregoryfenton over 10 years ago

    May I interject and offer an opinion here?

    Consider the time taken to monitor this thread, probe the board and buy all the parts necessary to follow advice offered here.

    How long before your costs (including an hourly rate) outweigh the value of what amounts to a throwaway computer?

    One of the aims of the Raspberry Pi project was to put computers in the hands of children and were designed to be cheap to replace when careless hands did something that resulted in a dead board.

     

    Greg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to gregoryfenton

    Greg, the time vs real dollars tradeoff can be very different for other people.

     

    On the other hand, there is a learning experience which will be useful at a  later date but the value currently is unknown.

     

    Mauricio: The LM1117-1.8 is a reaonsable LDO to make 1.8V from the 5V. Similarly the LM1117-3.3 is a good one for the 3.3V rail. In fact rpi-1 used one for the 3.3V rail. [update: And for the 1.8V rail as well!). Take care that you put the recommended capacitors near the LM1117. Check the datasheet for the VENDOR that you're using. TI might have other recommendations than ST for example.

     

    Finding a place to inject 3.3V is easy: The GPIO will do fine.

     

    Finding a place to inject 1.8V is more difficult. Hmm... Can you find C108, R57 and R58? Either side of R57 or C108 will do, but R58 being "not fitted" may be easier to solder to. (the other side of R58 is GND. Can you find C8 near there? One side is GND the other is 1.8V. Might be a lot bigger than the other ones.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Thank you for the reminder! It's at 0.40v.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    Hi Mauricio,

    This is an interesting finding.

    It seems both the 1.2 and 1.8V rails are quite ok in your case. However, the 3.3V rail being so low is not good. There are many chips on the board using the 3.3V power rail. If the CPU is getting really hot when powering the board, then it is probably gone. What about the ethernet and USB hub chip? This the one with the SMSC logo onto it. Is this chip getting hot too?

    Other ideas would include to desolder L1, which is the inductor used by the 3.3V regulator. By doing so, you will disconnect the 3.3V rail. If afterwards, the 5V rail is quite normal (the voltmeter readings should show a value close to 5V), then this means the fault is only in the 3.3V rail and it can be in one or more chips using it.

    To definitely know which chips are faulty, you can power the board from USB (having the L1 inductor disconnected, thus the board's 3.3V switching regulator won't interfere) and then connect an external 3.3V power supply (you can connect it at the point where you should have 3.3V) capable of delivering a few amps (at least). Then, all the faulty chips should get very hot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to bbolo1

    With the 3.3V at 0.4V the SMSC chip (the lan chip) will not be powered. It is powered only from the 3.3V rail. So with the power rail at 0.4V, it doesn't have the power to become hot.

     

    The 3.3V is used by:

    * the lan chip. (main power).

    * the SD card (main power)

    * the CPU (as IO voltage).

     

    If you have a lab power supply, setting the voltage to 3.3V and the current to say 40mA, remove the SD card  and power the 3.3V rails through the GPIO pins. If it goes into current limit that might be the LAN chip which might not even be broken. Increase the current to about 100mA. It should stay below that. All this of course afteryou've disconnected the regulator from the 3.3V by removing L1. as bbolo1 suggests.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Ok so, I tried to power it through my home plug and the 5v (red ones) are now at 4.85v, and all the others stayed the same voltages. All chips gets hot( they feel pretty much the same temperature). I didn't tried to desolder anything since the new voltage for the 5v changed. Should I still desolder anything or plans changed?

     

    @Roger Wolff I don't have a lab power supply, for now I can use a battery right? I can perhaps buy a low mA battery. Are lab power supply really usefull?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    Yes, lab power supplies are really useful!

     

    (note that you mentioned the word "really" and I answered with the word "really" in my response. Those are different meanings of a word spelled and written the same. Think about it. :-) )

     

    A lab powersupply has a configurable current limit. This means that you can set that limit at say 30% above what you expect your circuit to use, and then not blow stuff up if there is a mistake in a circuit.

     

    Example: I'm working on a motor-control-PCB. During startup, the CPU apparently tells the powerstage: connect V+ to motor pin A, while at the same time: connect GND to motor pin A. Of course that should never happen, but apparently it happens during startup. So far the "current limit" led of the powersupply blinks an instant and nothing blows up. If I connect a good LIPO battery as the powersupply I'm pretty sure that the FET switches would blow up.

     

    If you say that your chips get hot, that means that something is seriously wrong. A hint that nothing more can be done.

    If you still measure 0.4V on the 3.3V line, then it is very difficult for the LAN chip to become hot: It doesn't have any power. I question the observation....

     

    If the 3.3V line is "shorted" to GND (about 0.4V) by the regulator, then I can imagine the CPU getting hot. It MIGHT have a diode from its 1.2V supply to the 3.3V IO voltage. Normally not conductive, but now suddenly a current can flow.

     

    Many people confuse mAh ratings and mA ratings of batteries. I have a 3Ah LIPO battery rated at 120A. It can deliver 3A for an hour, or say 0.3A for 10 hours. But it can also deliver 120A for about 1/40th of an hour (90 seconds). Take a 10x smaller version of that battery and it says "300mAh", and you'd think: find that won't harm my 'pi. But it can deliver 12A, quite a lot end easily enough to damage a 'pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to rew

    Roger Wolff wrote:

     

    A lab powersupply has a configurable current limit. This means that you can set that limit at say 30% above what you expect your circuit to use, and then not blow stuff up if there is a mistake in a circuit.

    Yes, that is an extremely useful feature.  Another fun thing you can do with a lab supply is to clear a thin conductive bridge that's shorting together two signals because of a PC board defect.  You set your lab supply voltage to 0.5V or so and set the current way up to 10A or so.  Then you connect the leads to the two signals.  If the bridge is thin enough, the 10A will blow the bridge like a fuse and the 0.5V makes sure you don't apply too much voltage when the short clears.  This only works for some shorts, but when it works it rescues a board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to johnbeetem

    Absolutely. Did exactly that a week or two ago. Although my lab powersupply does not go any further than 3A, but it worked. :-)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    Thanks for the info image . On another notes, I took my meat thermometer to calculate the temperature of the chip and it reached up to 28°C (around 80°F).

    Yea I'm definitively that kind of person xd i'll read more about batteries. Do you suggest me to power up them with an external battery, or can I desolder anything, or change the diodes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    28°C is kind of normal. The normal operation of the RPi CPU can get higher than this value.

    The idea here is to use a 3.3V power supply capable of delivering at least a few amps. Then, by disconnecting the L1 (to disconnect the 3.3V switching regulator output) and using an external more powerful 3.3V power supply, you should be able to tell which chips are definitely fried. The faulty chips should get really hot (more than 60-80°C).

    If the main CPU is fried, you might cut the PCB area with the switching power supply and use it for future projects whenever you need 3.3, 1.8 or 1.2V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Hi!

    ok so at first, I tried to desolder it, and damn it was hard to, so I was scared to touch the others things around it. I ended up by breaking L1 carefully and then I was able to put some rosin core on it to make it easier for me to conduct things up. Can you tell me where am I supposed to join things? like the + and -  of the 3.3v battery.

    I'm going to attache some photos. Would you be able to tell me if I did a good or if I did not x.x

     

    Thanks!

    image

    The picture got rotated.. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Hi!

    ok so at first, I tried to desolder it, and damn it was hard to, so I was scared to touch the others things around it. I ended up by breaking L1 carefully and then I was able to put some rosin core on it to make it easier for me to conduct things up. Can you tell me where am I supposed to join things? like the + and -  of the 3.3v battery.

    I'm going to attache some photos. Would you be able to tell me if I did a good or if I did not x.x

     

    Thanks!

    image

    The picture got rotated.. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    Before going any further, just make sure you have a regulated 3.3V supply (have a powerful 3.3V LDO on your battery so it will have enough amps to supply).

    Now, put the "-" to any "GND" point on the board and the +3.3V to the upper part of the capacitor that filters the 3.3V rail (marked in orange).

    Then, power up the board using a USB power adapter. The switching regulators will supply the 1.2V and the 1.8V rails.

    Afterwards, connect your 3.3V power supply and check which chips are getting really hot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to bbolo1

    Note that "really hot" is much hotter than the 28 degrees that I remember that you measured.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to bbolo1

    Sorry for late responding, hope you guys had a good holiday. So I followed your instructions; the hottest chip was smsc, then broadcom, and finally the elpida. The smsc actually gave me electric shock or something I might of touch something else but it really got hot and I felt an electric shock. the other two were pretty much the same as before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    http://elinux.org/R-Pi_Troubleshooting#Power_.2F_Start-up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bbolo1
    0 bbolo1 over 10 years ago in reply to e14 Contributor

    Using a hot air gun, you can try to desolder the SMSC chip. Afterwards just make sure the pads on the PCB where the SMSC chip used to stay are clean and they don't make any shorts between them. Afterwards, you can try to power the board with all the voltages (1.2, 1.8, 3.3 and 5V) and see if the CPU is still functional.