Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is my raspberry unrepairable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 64 replies
  • Answers 2 answers
  • Subscribers 714 subscribers
  • Views 11943 views
  • Users 0 members are here
  • raspberry_pi
Related

Is my raspberry unrepairable?

e14 Contributor
e14 Contributor over 10 years ago

First of all I'm a beginner, so please don't judge me I know I did something bad.

 

SO, yesterday I was trying to make my raspberry pi 2 B to work with an external battery. I took a lithium polymer battery with 3.7v and 2500mah and I connect it to a booster. At first I was trying to hook it up to the micro usb input on the board and it didn't work. Then I look in youtube and I saw people plugging external batteries into the gpio pins. I joined the positive cable into the the first 5v pin and the negative cord into the first 3.3v pin and vs. Although when I connected the positive cable into the first 5v pin and the negative into the 3.3v pin for the second time with longer time touching them, it sparked and then I saw it left a kind of cut in both gpio pins. Now this morning that I try to power up my raspberry with a normal micro usb cable, I can feel the board getting warm(normal warm) but the led does not turn on.

 

In the pictures attached, the voltmeter says 4.12 v output but yesterday I adjust it to 5.2v also using the voltmeter but I don't know why it shows 4.12v now... And also in the mark on gpio is the same in the other side (the first 3.3v pin).

 

Is there anything I can do? Or is it burnout forever?

 

Thanks in advance.

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You have most lightly blown something on the PI

     

    The 4.3V battery should NOT have been connected between the 3.3V pin and the 5V pin, these are both seperate power + rails for parts of the PI board and you just put effectivly 8V into the 5V pin or caused excessive current to flow through pins not designed to have a difference of the battery or booster voltage.

     

    What you should have done is connect the batter or booster output to 0V for the black wire and 5V for the red one (Using the booster to give you the 5V

     

    you best option is actually to feed the 5V into the PI via the USB connection though, so battery to booster, booster to PI USB power connector

     

    the schamatics have not been published but based on your description of how you connected a battery capapable of providing many amps between the 3V3 and 5V pins I would expect something to have failed

     

    Sorry for the bad news, may the PI RIP.

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to Robert Peter Oakes

    So I cannot replace anything (nothing has physical damage except the pins, so I thought I may be able to replace them or even replace the led xd)? And one more question how can I put the black cable to 0v (because both cable where fused with the + and - of the boost output) ?

     

    Thank for the fast responding! :O

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dwinhold
    0 dwinhold over 10 years ago in reply to e14 Contributor

    I have done something simular by accident, the Raspberry isn't repairable. I use mine to show people what they look like. At least I don't worry about them dropping it. Sorry about the misfortune...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dwinhold
    0 dwinhold over 10 years ago in reply to e14 Contributor

    I have done something simular by accident, the Raspberry isn't repairable. I use mine to show people what they look like. At least I don't worry about them dropping it. Sorry about the misfortune...