Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rpi2 + Cirrus/Element14 Audio Board + Arch Linux
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 674 views
  • Users 0 members are here
Related

Rpi2 + Cirrus/Element14 Audio Board + Arch Linux

e14 Contributor
e14 Contributor over 10 years ago

This is my first post here, hopefully this is in the right place.

 

I have an Rpi2 and the Cirrus/Element14 Audio board.  I've been able to make it work under raspbian Linux (kernel 4.1.13) using the precompiled kernel from hiassoft (thank you!)

 

I prefer Arch Linux and have spent time searching for posts regarding using the audio board with Arch Linux and I've found nothing I can use.

 

So I started my own little adventure.  Since the kernels are both version 4.1.13, I thought it might be possible to get the board working with Arch Linux using the precompiled kernel.  My first attempt basically followed the same procedure as for raspbian, that is, to expand the tar file at the file system root and then edit the two files that need special attention.  The first time I did this with Arch Linux, the tar file extract deleted the link from /lib to /usr/lib which broke a lot of things and of course, did not work.  Once I realized what happened, I tried something a bit different - I extracted the tar file to a benign location and then used cp -a to copy the files to /usr/lib and then I edited the two files.  When I rebooted, the red LED went out (which also happened in raspbian - which worked).  So I installed mplayer in Arch, but it wouldn't play an mp3 that played with raspbian.  An error message was printed that said something like:   The sound card got stuck!

 

Anyway, this is as far as I can go with this, I hope maybe this is helpful to someone else.

 

The question is - has anyone successfully made the Cirrus/Element14 Audio board work with Arch Linux?

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 10 years ago

    jovianpyx wrote:

     

    When I rebooted, the red LED went out (which also happened in raspbian - which worked).

    The red led indicates: "power supply OK: we have more than 4.65V where 5V should be present".

     

    The 'pi will work down to 3.3V, but peripherals like USB keyboards or HDMI->VGA converters might require something closer to 5V at that location. It's a warning if the red led goes out. As long as everything works, don't worry about it. But in your case it doesn't work. So, to eliminate possible causes I would suggest you look at your "power supply". This includes the cable that you use to connect to the 'pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rew
    0 rew over 10 years ago

    jovianpyx wrote:

     

    When I rebooted, the red LED went out (which also happened in raspbian - which worked).

    The red led indicates: "power supply OK: we have more than 4.65V where 5V should be present".

     

    The 'pi will work down to 3.3V, but peripherals like USB keyboards or HDMI->VGA converters might require something closer to 5V at that location. It's a warning if the red led goes out. As long as everything works, don't worry about it. But in your case it doesn't work. So, to eliminate possible causes I would suggest you look at your "power supply". This includes the cable that you use to connect to the 'pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    My bad - there is more than one red LED.  The red LED on the Rpi2 remains illuminated at all times, the red LED on the Cirrus audio board goes out when it's driver loads.