Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Microstack GPS and Accelerometer on RaspberryPi 2 and Ubuntu Mate
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 2173 views
  • Users 0 members are here
  • Ubuntu
  • 2
  • rasberrypi
  • raspberry_pi
  • mate
  • microstack
Related

Microstack GPS and Accelerometer on RaspberryPi 2 and Ubuntu Mate

doubletop
doubletop over 10 years ago

I'm going round in circles trying to get this to work with Ubuntu Mate and its not clear which posts on any website are relevant and which are not.

 

Here's where I've got to.

 

$ sudo apt-get install python3-microstacknode

 

Doesn't work

 

sudo apt-get install python3-pip

 

works

 

sudo pip-3.2 install microstackcommon microstacknode

 

works if pip-3.2 is changed to pip. However it puts all the files into /usr/local/lib rather than /usr/lib and there are no example files. microstackcommon and microstacknode files have been moved to /usr/lib/ in the existing file structure for python 2.7 python3,4 and python3,5. I got the examples from GitHUb and placed them in a local folder.

 

As there is no Rasp-config available config.txt has been edited to add

 

sudo nano /boot/config.txt

 

and

 

dtparam=i2c_arm=on

dtparam=spi=on

 

sudo i2cdetect -y 1

 

works. However, no device is found

 

0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:      -- -- -- -- -- -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --

 

Running the examples accelcat.py

 

Traceback (most recent call last):

  File "/home/pete/PythonTest/accelcat.py", line 11, in <module>

    with MMA8452Q() as accelerometer:

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 126, in __enter__

    self.init()

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 131, in init

    self.standby()

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 153, in standby

    self.ctrl_reg1.set(self._ctrl_reg1_value)

  File "/usr/lib/python3.4/dist-packages/microstacknode/hardware/accelerometer/mma8452q.py", line 279, in set

    writing_bytes(self.device_address, self.register_address, v))

  File "/usr/lib/python3.4/dist-packages/microstackcommon/i2c.py", line 85, in transaction

    ioctl(self.fd, I2C_RDWR, ioctl_arg)

OSError: [Errno 5] Input/output error

 

and gpscat.py

 

Traceback (most recent call last):

  File "/home/pete/PythonTest/gpscat.py", line 3, in <module>

    import microstacknode.gps.l80gps

ImportError: No module named 'microstacknode.gps'

 

 

So clearly something is missing  from the pip install so rather than editing and juggling around files please where or how do I find the 'proper' install package that gets everything i need to make this work with Ubuntu Mate?

 

Pete

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to clem57

    http://docz.io/doc/58441/microstack%E2%84%A2-gps-getting-started

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • doubletop
    0 doubletop over 10 years ago

    Thanks for your efforts Clem I'd found those references. However, I’ve just found this one and now I'm getting basic data in Python3.4 if I run Python as root.

     

    https://www.raspberrypi.org/forums/viewtopic.php?f=41&t=113155

     

    At the moment I don't have user rights to set up /dev/ttyAMA0 buts that’s a problem with my setup

     

    Basically its nothing to do with running it under Ubuntu Mate. The whole thing is a mess that Microstack need to get tidied up and the documentation updated and clear information about the missing jumper on the accelerometer cards.

     

    Until they do that and unless you like a bit of a challenge I'd keep well clear of the Microstack products


    Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<